Hi,
We are using the imx8mm with our custom board loaded with Android 11. Also added ov5640 camera support.
csi_mclk: csi-mclk {
compatible = "pwm-clock";
#clock-cells = <0>;
clock-frequency = <20000000>;
clock-output-names = "csi_mclk";
pwms = <&pwm4 0 50>; /* 1 / 50 ns = 20 MHz */
};
&i2c4c {
ov5640-mipi1@3c {
AVDD-supply = <®_ldo3>;
DOVDD-supply = <®_vref_1v8>;
DVDD-supply = <®_vref_3v3>;
clocks = <&csi_mclk>;
clock-names = "xclk";
compatible = "ovti,ov5640_mipisubdev";
csi_id = <0>;
mclk = <20000000>;
mipi_csi;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c4_ov5640_mipi>;
powerdown-gpios = GP_OV5640_MIPI_POWER_DOWN;
reg = <0x3c>;
reset-gpios = GP_OV5640_MIPI_RESET;
status = "okay";
port {
ov5640_mipi1_ep: endpoint {
remote-endpoint = <&mipi1_ov5640_ep>;
};
};
};
};
&mipi_csi_1 {
#address-cells = <1>;
#size-cells = <0>;
status = "okay";
port {
mipi1_ov5640_ep: endpoint@1 {
remote-endpoint = <&ov5640_mipi1_ep>;
data-lanes = <2>;
csis-hs-settle = <13>;
csis-clk-settle = <2>;
csis-wclk;
};
csi1_mipi_ep: endpoint@2 {
remote-endpoint = <&csi1_ep>;
};
};
};
&csi1_bridge {
fsl,mipi-mode;
status = "okay";
port {
csi1_ep: endpoint {
remote-endpoint = <&csi1_mipi_ep>;
};
};
};
We are facing an issue while capturing a 5mp image with ov5640. We have observed a delay of 1s between the time the capture button clicked vs the image capture happened. Hence the frames that we got are different from what we wanted.
10-11 11:15:08.384 2933 2933 D CAM_LcyLocProvider: No location received yet.
10-11 11:15:08.401 2933 3005 D CAM_CommandExecutor: Executing command: PictureTakerCommand{command=com.android.camera.one.v2.photo.SimpleImageCaptureCommand@1c64da7} START
10-11 11:15:08.411 2933 2933 V CAM_CameraActivity: onSessionQueued: camera_session://google.com/4c388a54-1251-4620-beed-53eaa1b909a5
10-11 11:15:08.414 2933 2933 V CAM_FilmstripView: suggesting item bounds: 640x886
10-11 11:15:08.415 2933 2933 V CAM_FilmstripView: getRecycledView, recycled=false
10-11 11:15:08.419 2933 2933 V CAM_FilmstripView: recycleView
10-11 11:15:08.421 2933 2933 I CAM_FilmstripView: [ViewItem:0] mData.renderThumbnail()
10-11 11:15:08.422 2933 2933 D CAM_FilmstripView: onFilmstripItemInserted()
10-11 11:15:08.447 415 452 I gralloc_driver: is_supported check descriptor name=ImageReader-2592x1944f100m15-2933-0, width=8388608, height=1, droid_format=BLOB, usage=CAMERA_OUTPUT|CPU_READ_OFTEN|GPU_RE
10-11 11:15:08.482 412 1813 I CameraDeviceSessionHwlImpl: PickConfigStream: previewIdx 1, callbackIdx -1, stillcapIdx 0, recordIdx -1, intent 2
10-11 11:15:08.482 412 1813 I CameraDeviceSessionHwlImpl: choose stream index 0 as config stream
---------diff--------
10-11 11:15:08.482 412 1813 I MMAPStream: onDeviceStopLocked
10-11 11:15:08.484 412 1813 I MMAPStream: onDeviceConfigureLocked
10-11 11:15:08.484 412 1813 I MMAPStream: onDeviceConfigureLocked, Width * Height 2592 x 1944 format YUYV, fps: 30, capturemode 5
----------------------
10-11 11:15:08.940 412 1813 I VideoStream: postConfigure, set omit frames 2 for 2592x1944
---------diff--------
10-11 11:15:08.940 412 1813 I MMAPStream: onDeviceStartLocked
10-11 11:15:08.954 412 1813 I MMAPStream: onDeviceStartLocked, register buffer, phy 0x94200000, virt 0xf5733b42a000, size 10077696
10-11 11:15:08.960 412 1813 I MMAPStream: onDeviceStartLocked, register buffer, phy 0x94c00000, virt 0xf5733aa8d000, size 10077696
10-11 11:15:08.960 412 1813 I MMAPStream: onDeviceStartLocked VIDIOC_QBUF phy:0x94200000
10-11 11:15:08.960 412 1813 I MMAPStream: onDeviceStartLocked VIDIOC_QBUF phy:0x94c00000
----------------------
10-11 11:15:08.997 585 1298 I system_server: oneway function results will be dropped but finished with status OK and parcel size 4
10-11 11:15:08.998 585 1011 I system_server: oneway function results will be dropped but finished with status OK and parcel size 4
10-11 11:15:08.999 429 2714 D AF::TrackHandle: OpPlayAudio: track:63 usage:13 not muted
10-11 11:15:09.001 2933 2933 I AudioTrack: createTrack_l(0): AUDIO_OUTPUT_FLAG_FAST successful; frameCount 0 -> 20073
10-11 11:15:09.001 585 1011 I system_server: oneway function results will be dropped but finished with status OK and parcel size 8
10-11 11:15:09.004 585 1011 I system_server: oneway function results will be dropped but finished with status OK and parcel size 4
10-11 11:15:09.005 406 1238 W audio_hw_primary: ret -32, pcm write 768 error wait error: hw 0xdec0 app 0xe4c0 avail 0x0
10-11 11:15:09.005 406 1238 W audio_hw_primary: : Broken pipe
---------diff--------
10-11 11:15:09.147 412 2997 I MMAPStream: onFrameAcquireLocked omit frame
10-11 11:15:09.214 412 2997 I MMAPStream: onFrameAcquireLocked omit frame
----------------------
10-11 11:15:09.348 412 2997 E CameraUtils: Error: getSizeByForamtRes format 0x21 not supported
10-11 11:15:09.349 412 2997 E JpegBuilder: Invalid GPS coordinate
10-11 11:15:09.349 412 2997 E JpegBuilder: Invalid GPS coordinate
10-11 11:15:09.349 412 2997 E CameraMetadata: Get: error reading tag
10-11 11:15:09.349 412 2997 E CameraMetadata: Get: error reading tag
10-11 11:15:09.548 412 2997 I CameraDeviceSessionHwlImpl: processJpegBuffer, dstbuf size 8388608, 10119168, jpeg_size 3550669, max jpeg size 8388608
10-11 11:15:09.553 412 412 I CameraDeviceSessionHwlImpl: PickConfigStream: previewIdx 1, callbackIdx -1, stillcapIdx 0, recordIdx -1, intent 1
10-11 11:15:09.553 412 412 I CameraDeviceSessionHwlImpl: choose stream index 1 as config stream
---------diff---------
10-11 11:15:09.554 412 412 I MMAPStream: onDeviceStopLocked
10-11 11:15:09.560 412 412 I MMAPStream: onDeviceConfigureLocked
10-11 11:15:09.560 412 412 I MMAPStream: onDeviceConfigureLocked, Width * Height 640 x 480 format YUYV, fps: 30, capturemode 0
-----------------------
10-11 11:15:09.561 2933 2933 V CAM_CaptureModule: AF status is state:INACTIVE
---------diff---------
10-11 11:15:09.760 412 412 I MMAPStream: onDeviceStartLocked
10-11 11:15:09.766 412 412 I MMAPStream: onDeviceStartLocked, register buffer, phy 0x8e600000, virt 0xf5734bf70000, size 614400
10-11 11:15:09.767 412 412 I MMAPStream: onDeviceStartLocked, register buffer, phy 0x8ea00000, virt 0xf57348069000, size 614400
10-11 11:15:09.768 412 412 I MMAPStream: onDeviceStartLocked, register buffer, phy 0x8eb00000, virt 0xf57347fd3000, size 614400
10-11 11:15:09.768 412 412 I MMAPStream: onDeviceStartLocked VIDIOC_QBUF phy:0x8e600000
10-11 11:15:09.768 412 412 I MMAPStream: onDeviceStartLocked VIDIOC_QBUF phy:0x8ea00000
10-11 11:15:09.768 412 412 I MMAPStream: onDeviceStartLocked VIDIOC_QBUF phy:0x8eb00000
-----------------------
10-11 11:15:09.807 2933 3005 D CAM_ProcessingSvcMgr: Task added. Queue size now: 1
10-11 11:15:09.810 585 1011 W ActivityManager: Unable to start service Intent { cmp=com.android.camera2/com.android.camera.processing.ProcessingService } U=0: not found
10-11 11:15:09.811 2933 3005 V CAM_ImageBackend: Received an opened image: 1/0
10-11 11:15:09.811 2933 3005 V CAM_ImageBackend: Setting an image reference count of 1 Total refs = 1
10-11 11:15:09.813 2933 3005 D CAM_CommandExecutor: Executing command: PictureTakerCommand{command=com.android.camera.one.v2.photo.SimpleImageCaptureCommand@1c64da7} END
10-11 11:15:09.838 2933 3013 V CAM_ImageBackend: Ref release. Total refs = 0
10-11 11:15:09.839 2933 3013 V CAM_ImageBackend: Ref release close.
10-11 11:15:09.839 2933 3014 E ion : ioctl c0044901 failed with code -1: Inappropriate ioctl for device
10-11 11:15:09.841 2933 3014 V CAM_ImageBackend: Release of image occurred. Good fun. Total Images Open/Closed = 1/1
10-11 11:15:09.894 2933 2933 V CAM_CaptureModule: AF status is state:PASSIVE_SCAN
10-11 11:15:09.895 2933 2933 V CAM_FocusController: Running showPassiveFocusAtCenter()
10-11 11:15:09.896 2933 2933 I CAM_FocusRingView: Computing center via preview size.
10-11 11:15:09.949 0 0 W healthd : battery l=100 v=4404 t=20.0 h=2 st=5 c=1 chg=a
10-11 11:15:10.040 2933 2952 D CompatibilityChangeReporter: Compat change id reported: 150939131; UID 10098; state: DISABLED
10-11 11:15:10.041 2933 2981 V CAM_CameraDataAdapter: updating media metadata with photos newer than id: 76
10-11 11:15:10.053 1302 2414 W SQLiteQueryBuilder: Allowing abusive custom column: LIKE
10-11 11:15:10.054 1302 2414 W SQLiteQueryBuilder: Allowing abusive custom column: AND
10-11 11:15:10.054 1302 2414 W SQLiteQueryBuilder: Allowing abusive custom column: DESC
10-11 11:15:10.066 2933 2981 W CAM_PhotoDataFact: Zero dimension in ContentResolver for /storage/emulated/0/DCIM/Camera/IMG_20221011_111508.jpg:0x0
10-11 11:15:10.069 2933 2981 D skia : --- Failed to create image decoder with message 'unimplemented'
10-11 11:15:10.090 2933 2981 W CAM_PhotoDataFact: Dimension decode failed for /storage/emulated/0/DCIM/Camera/IMG_20221011_111508.jpg
10-11 11:15:10.130 1302 2414 W SQLiteQueryBuilder: Allowing abusive custom column: AND
10-11 11:15:10.130 1302 2414 W SQLiteQueryBuilder: Allowing abusive custom column: IN
10-11 11:15:10.168 2933 3013 D StrictMode: StrictMode policy violation: android.os.strictmode.ContentUriWithoutPermissionViolation: content://media/external/images/media/77 exposed beyond app through Int?
10-11 11:15:10.168 2933 3013 D StrictMode: at android.os.StrictMode.onContentUriWithoutPermission(StrictMode.java:2149)
10-11 11:15:10.168 2933 3013 D StrictMode: at android.net.Uri.checkContentUriWithoutPermission(Uri.java:2403)
10-11 11:15:10.168 2933 3013 D StrictMode: at android.content.Intent.prepareToLeaveProcess(Intent.java:11164)
10-11 11:15:10.168 2933 3013 D StrictMode: at android.content.Intent.prepareToLeaveProcess(Intent.java:11104)
10-11 11:15:10.168 2933 3013 D StrictMode: at android.app.ContextImpl.sendBroadcast(ContextImpl.java:1114)
10-11 11:15:10.168 2933 3013 D StrictMode: at android.content.ContextWrapper.sendBroadcast(ContextWrapper.java:468)
10-11 11:15:10.168 2933 3013 D StrictMode: at com.android.camera.util.CameraUtil.broadcastNewPicture(CameraUtil.java:749)
10-11 11:15:10.168 2933 3013 D StrictMode: at com.android.camera.session.PlaceholderManager.finishPlaceholder(PlaceholderManager.java:140)
10-11 11:15:10.168 2933 3013 D StrictMode: at com.android.camera.session.CaptureSessionImpl.saveAndFinish(CaptureSessionImpl.java:322)
10-11 11:15:10.168 2933 3013 D StrictMode: at com.android.camera.processing.imagebackend.TaskCompressImageToJpeg.run(TaskCompressImageToJpeg.java:344)
10-11 11:15:10.168 2933 3013 D StrictMode: at com.android.camera.processing.imagebackend.ImageBackend$TaskDoneWrapper.run(ImageBackend.java:829)
10-11 11:15:10.168 2933 3013 D StrictMode: at java.util.concurrent.ThreadPoolExecutor.runWorker(ThreadPoolExecutor.java:1167)
10-11 11:15:10.168 2933 3013 D StrictMode: at java.util.concurrent.ThreadPoolExecutor$Worker.run(ThreadPoolExecutor.java:641)
10-11 11:15:10.168 2933 3013 D StrictMode: at java.lang.Thread.run(Thread.java:923)
10-11 11:15:10.168 2933 3013 D StrictMode: at com.android.camera.async.AndroidPriorityThread.run(AndroidPriorityThread.java:26)
10-11 11:15:10.181 2933 3013 D StrictMode: StrictMode policy violation: android.os.strictmode.ContentUriWithoutPermissionViolation: content://media/external/images/media/77 exposed beyond app through Int?
10-11 11:15:10.181 2933 3013 D StrictMode: at android.os.StrictMode.onContentUriWithoutPermission(StrictMode.java:2149)
10-11 11:15:10.181 2933 3013 D StrictMode: at android.net.Uri.checkContentUriWithoutPermission(Uri.java:2403)
10-11 11:15:10.181 2933 3013 D StrictMode: at android.content.Intent.prepareToLeaveProcess(Intent.java:11164)
10-11 11:15:10.181 2933 3013 D StrictMode: at android.content.Intent.prepareToLeaveProcess(Intent.java:11104)
10-11 11:15:10.181 2933 3013 D StrictMode: at android.app.ContextImpl.sendBroadcast(ContextImpl.java:1114)
10-11 11:15:10.181 2933 3013 D StrictMode: at android.content.ContextWrapper.sendBroadcast(ContextWrapper.java:468)
10-11 11:15:10.181 2933 3013 D StrictMode: at com.android.camera.util.CameraUtil.broadcastNewPicture(CameraUtil.java:751)
10-11 11:15:10.181 2933 3013 D StrictMode: at com.android.camera.session.PlaceholderManager.finishPlaceholder(PlaceholderManager.java:140)
10-11 11:15:10.181 2933 3013 D StrictMode: at com.android.camera.session.CaptureSessionImpl.saveAndFinish(CaptureSessionImpl.java:322)
10-11 11:15:10.181 2933 3013 D StrictMode: at com.android.camera.processing.imagebackend.TaskCompressImageToJpeg.run(TaskCompressImageToJpeg.java:344)
10-11 11:15:10.181 2933 3013 D StrictMode: at com.android.camera.processing.imagebackend.ImageBackend$TaskDoneWrapper.run(ImageBackend.java:829)
10-11 11:15:10.181 2933 3013 D StrictMode: at java.util.concurrent.ThreadPoolExecutor.runWorker(ThreadPoolExecutor.java:1167)
10-11 11:15:10.181 2933 3013 D StrictMode: at java.util.concurrent.ThreadPoolExecutor$Worker.run(ThreadPoolExecutor.java:641)
10-11 11:15:10.181 2933 3013 D StrictMode: at java.lang.Thread.run(Thread.java:923)
10-11 11:15:10.181 2933 3013 D StrictMode: at com.android.camera.async.AndroidPriorityThread.run(AndroidPriorityThread.java:26)
10-11 11:15:10.193 2933 2933 V CAM_CameraActivity: onSessionDone:camera_session://google.com/4c388a54-1251-4620-beed-53eaa1b909a5
10-11 11:15:10.200 1302 1322 W SQLiteQueryBuilder: Allowing abusive custom column: LIKE
10-11 11:15:10.200 1302 1322 W SQLiteQueryBuilder: Allowing abusive custom column: AND
10-11 11:15:10.200 1302 1322 W SQLiteQueryBuilder: Allowing abusive custom column: DESC
10-11 11:15:10.218 585 638 I DropBoxManagerService: add tag=system_app_strictmode isTagEnabled=true flags=0x2
10-11 11:15:10.231 2933 2933 I CAM_FilmstripView: [ViewItem:0] mData.renderTiny()
10-11 11:15:10.233 2933 2933 V CAM_FilmstripView: updateViewItem() - recycling old data item and setting new
10-11 11:15:10.239 2933 2933 D CAM_FilmstripView: updateViewItem(bufferIndex: 2)
10-11 11:15:10.239 2933 2933 D CAM_FilmstripView: updateViewItem() - mIsUserScrolling: false
10-11 11:15:10.240 2933 2933 D CAM_FilmstripView: updateViewItem() - mController.isScrolling() - false
10-11 11:15:10.240 2933 2933 I CAM_FilmstripView: [ViewItem:0] mData.renderThumbnail()
10-11 11:15:10.263 1302 1322 W MediaProvider: Using FUSE for /storage/emulated/0/DCIM/Camera/IMG_20221011_111508.jpg
10-11 11:15:10.266 1302 1347 W SQLiteQueryBuilder: Allowing abusive custom column: AND
10-11 11:15:10.307 1302 1347 W MediaProvider: Using FUSE for /storage/emulated/0/DCIM/Camera/IMG_20221011_111508.jpg
10-11 11:15:10.313 1302 2414 W MediaProvider: Using FUSE for /storage/emulated/0/DCIM/Camera/IMG_20221011_111508.jpg
10-11 11:15:10.326 1302 1347 W MediaProvider: Using FUSE for /storage/emulated/0/DCIM/Camera/IMG_20221011_111508.jpg
But when we change the capture options to .3mp this delay is not seen.
What could be the cause of this issue?