decode jpeg images.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

decode jpeg images.

跳至解决方案
2,014 次查看
omerlevin
Contributor I

Hello, I am trying to decode JPEG images using "Line buffer Mode". Reviewing the documentation in "i.MX 6Dual/6Quad VPU Application Programming Interface Linux Reference Manual" Rev L3.0.35_4.1.0, 09/2013, and the mxc_vpu_test (from LTIB) I have a few questions.

- It seems there are quite a few differences in the flow: The test is not setting DecOpenParam.jpgLineBufferMode, thus using a default value of 0, meaning (according to the documentation) 'Line-Buffer Mode". In this mode, according to the flowchart in <3.3.1.1>, functions vpu_DecUpdateBitstreamBuffer()/vpu_DecGetBitstreamBuffer() should only be called once at the start of decoding, and not per frame as done in the test code. Similar call is done to Vpu_DecStartOneFrame().

- According to the documentation, in line buffer mode (DecOpenParam.jpgLineBufferMode =0) There's a need to "set bitstream to bitstreambuffer start address" (p.43). How should that be done?

When trying to do it by transferring the decoder input stream to bitstreambuffer start address using vpu_DecUpdateBitstreamBuffer() or vpu_DecBitBufferFlush(), vpu_DecGetOutputInfo() returns with decodingSuccess=17 (vpu needs more bitstream in rollback mode).

My version info below.

Thanks in advance.

Omer

my version info

Product Info: i.MX6Q

VPU firmware version: 2.1.5_r32515

VPU library version: 5.4.6

标签 (1)
0 项奖励
回复
1 解答
1,808 次查看
omerlevin
Contributor I

I found the issue:

From the above mentioned documentation ("i.MX 6Dual/6Quad VPU Application Programming Interface Linux Reference Manual", last revision I've found is L3.0.35_4.1.0, 09/2013), 3.2.3 - DecOpenParam, for jpgLineBufferMode description it says:

"jpgLineBufferMode where 0 is a LineBuffer mode and 1 is a streaming mode."

But actually it's the opposite.

0 is a streaming mode.

1 is a LineBuffer mode.

I've tested it and seems to be working well. I will happy if someone from freescale will confirm and update the manual.

thanks

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,809 次查看
omerlevin
Contributor I

I found the issue:

From the above mentioned documentation ("i.MX 6Dual/6Quad VPU Application Programming Interface Linux Reference Manual", last revision I've found is L3.0.35_4.1.0, 09/2013), 3.2.3 - DecOpenParam, for jpgLineBufferMode description it says:

"jpgLineBufferMode where 0 is a LineBuffer mode and 1 is a streaming mode."

But actually it's the opposite.

0 is a streaming mode.

1 is a LineBuffer mode.

I've tested it and seems to be working well. I will happy if someone from freescale will confirm and update the manual.

thanks

0 项奖励
回复