de-interlance for yocto linux 5.10.9

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

de-interlance for yocto linux 5.10.9

跳至解决方案
1,369 次查看
simonlin
Contributor II

Hi @qiang_li-mpu_se 

Here is my environment

HW platform: imx8-qm, tw9992

OS: Yocto Linux 5.10.9

I try to post de-interlance mode in yocto linux 5.10.9, but the V4L2 data structure is different with  below reference article

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/ISL79987-and-adv7180-de-interlace-driver...

Do you have newer de-interlance patch for yocto linux 5.10.9 ?

Thanks

0 项奖励
回复
1 解答
1,356 次查看
qiang_li-mpu_se
NXP Employee
NXP Employee
0 项奖励
回复
3 回复数
1,357 次查看
qiang_li-mpu_se
NXP Employee
NXP Employee
0 项奖励
回复
1,361 次查看
simonlin
Contributor II

Hi @qiang_li-mpu_se 

That's good news

I look forward to get the patch

Thanks for your response

 

0 项奖励
回复
1,365 次查看
qiang_li-mpu_se
NXP Employee
NXP Employee

The patch for L5.4.70 BSP will be released in next week. 

0 项奖励
回复