de-interlance for yocto linux 5.10.9

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

de-interlance for yocto linux 5.10.9

ソリューションへジャンプ
1,370件の閲覧回数
simonlin
Contributor II

Hi @qiang_li-mpu_se 

Here is my environment

HW platform: imx8-qm, tw9992

OS: Yocto Linux 5.10.9

I try to post de-interlance mode in yocto linux 5.10.9, but the V4L2 data structure is different with  below reference article

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/ISL79987-and-adv7180-de-interlace-driver...

Do you have newer de-interlance patch for yocto linux 5.10.9 ?

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
1,357件の閲覧回数
qiang_li-mpu_se
NXP Employee
NXP Employee
0 件の賞賛
返信
3 返答(返信)
1,358件の閲覧回数
qiang_li-mpu_se
NXP Employee
NXP Employee
0 件の賞賛
返信
1,362件の閲覧回数
simonlin
Contributor II

Hi @qiang_li-mpu_se 

That's good news

I look forward to get the patch

Thanks for your response

 

0 件の賞賛
返信
1,366件の閲覧回数
qiang_li-mpu_se
NXP Employee
NXP Employee

The patch for L5.4.70 BSP will be released in next week. 

0 件の賞賛
返信