customer board kernel boot stuck at "Waiting for root device /dev/mmcblk0p2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

customer board kernel boot stuck at "Waiting for root device /dev/mmcblk0p2

Jump to solution
7,685 Views
listplot3d
Contributor III

I have modified uboot to boot from sd0 rather than sd1 on imx6ulevk board. then uboot passed, but kernel stuck at "Waiting for root device /dev/mmcblk0p2..." could anyone give me a hint?

Thanks & Best Regards

-Shawn

 

Below comparison used same sd card, which had uboot modified but evk kernel unmodified

Imx6ul EVK log

 

=> printenv

baudrate=115200

board_name=EVK

board_rev=14X14

boot_fdt=try

bootcmd=run findfdt;mmc dev ${mmcdev};mmc dev ${mmcdev}; if mmc rescan; then if run loadbootscript; then run bootscript; else if run loadimage; then run mmcboot; else run netboot; fi; fi; else run netboot; fi

bootcmd_mfg=run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};

bootdelay=3

bootscript=echo Running bootscript from mmc ...; source

console=ttymxc0

ethact=FEC1

ethaddr=00:04:9f:04:b4:c1

ethprime=FEC

fdt_addr=0x83000000

fdt_file=undefined

fdt_high=0xffffffff

findfdt=if test $fdt_file = undefined; then if test $board_name = EVK && test $board_rev = 9X9; then setenv fdt_file imx6ul-9x9-evk.dtb; fi; if test $board_name = EVK && test $board_rev = 14X14; then setenv fdt_file imx6ul-14x14-evk.dtb; fi; if test $fdt_file = undefined; then echo WARNING: Could not determine dtb to use; fi; fi;

image=zImage

initrd_addr=0x83800000

initrd_high=0xffffffff

ip_dyn=yes

loadaddr=0x80800000

loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};

loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}

loadimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${image}

mfgtool_args=setenv bootargs console=${console},${baudrate} rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.file=/fat g_mass_storage.ro=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber="" clk_ignore_unused

mmcargs=setenv bootargs console=${console},${baudrate} root=${mmcroot}

mmcautodetect=yes

mmcboot=echo Booting from mmc ...; run mmcargs; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootz ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;

mmcdev=1

mmcpart=1

mmcroot=/dev/mmcblk1p2 rootwait rw

netargs=setenv bootargs console=${console},${baudrate} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp

netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${image}; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if ${get_cmd} ${fdt_addr} ${fdt_file}; then bootz ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;

panel=TFT43AB

script=boot.scr

 

Environment size: 2457/8188 bytes

=> mmc list

FSL_SDHC: 0

FSL_SDHC: 1 (SD)

=> mmc part

Partition Map for MMC device 1  --   Partition Type: DOS

 

Part    Start Sector    Num Sectors     UUID            Type

  1     8192            16384           0aad0b47-01     0c

  2     24576           1949696         0aad0b47-02     83

=> mmc dev

switch to partitions #0, OK

mmc1 is current device

=>boot

usbcore: registered new interface driver ath3k

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci-pltfm: SDHCI platform and OF driver helper

/soc/aips-bus@02100000/usdhc@02190000: voltage-ranges unspecified

sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO

sdhci-esdhc-imx 2190000.usdhc: No vqmmc regulator found

mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA

/soc/aips-bus@02100000/usdhc@02194000: voltage-ranges unspecified

sdhci-esdhc-imx 2194000.usdhc: could not get ultra high speed state, work on normal mode

sdhci-esdhc-imx 2194000.usdhc: No vmmc regulator found

sdhci-esdhc-imx 2194000.usdhc: No vqmmc regulator found

mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA

caam 2140000.caam: Entropy delay = 3200

caam 2140000.caam: Instantiated RNG4 SH0

mmc1: host does not support reading read-only switch, assuming write-enable

caam 2140000.caam: Instantiated RNG4 SH1

caam 2140000.caam: device ID = 0x0a16030000000000 (Era -524)

caam 2140000.caam: job rings = 3, qi = 0

mmc1: new high speed SDHC card at address aaaa  #string from drivers/mmc/core/bus.c

mmcblk1: mmc1:aaaa SL32G 29.7 GiB

 mmcblk1: p1 p2

 

 

caam algorithms registered in /proc/crypto

caam_jr 2141000.jr0: registering rng-caam

can-3v3: disabling

ALSA device list:

  #0: wm8960-audio

EXT3-fs (mmcblk1p2): error: couldn't mount because of unsupported optional features (240)

EXT2-fs (mmcblk1p2): error: couldn't mount because of unsupported optional features (240)

EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)

VFS: Mounted root (ext4 filesystem) on device 179:2.

devtmpfs: mounted

Freeing unused kernel memory: 444K (80b29000 - 80b98000)

INIT: version 2.88 booting

Starting udev

udevd[175]: starting version 3.1.5

random: udevd urandom read with 14 bits of entropy available

EXT4-fs (mmcblk1p2): re-mounted. Opts: (null)

bootlogd: cannot allocate pseudo tty: No such file or directory

 

Imx costom board uboot environment

 

=> printenv

baudrate=115200

board_name=EVK

board_rev=14X14

boot_fdt=try

bootcmd=run findfdt;mmc dev ${mmcdev};mmc dev ${mmcdev}; if mmc rescan; then if run loadbootscript; then run bootscript; else if run loadimage; then run mmcboot; else run netboot; fi; fi; else run netboot; fi

bootcmd_mfg=run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};

bootdelay=3

bootscript=echo Running bootscript from mmc ...; source

console=ttymxc0

ethprime=FEC

 

 

fdt_addr=0x83000000

fdt_file=undefined

fdt_high=0xffffffff

findfdt=if test $fdt_file = undefined; then if test $board_name = EVK && test $board_rev = 9X9; then setenv fdt_file imx6ul-9x9-evk.dtb; fi; if test $board_name = EVK && test $board_rev = 14X14; then setenv fdt_file imx6ul-14x14-evk.dtb; fi; if test $fdt_file = undefined; then echo WARNING: Could not determine dtb to use; fi; fi;

image=zImage

initrd_addr=0x83800000

initrd_high=0xffffffff

ip_dyn=yes

loadaddr=0x80800000

loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};

loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}

loadimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${image}

mfgtool_args=setenv bootargs console=${console},${baudrate} rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.file=/fat g_mass_storage.ro=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber="" clk_ignore_unused

mmcargs=setenv bootargs console=${console},${baudrate} root=${mmcroot}

mmcautodetect=yes

mmcboot=echo Booting from mmc ...; run mmcargs; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootz ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;

mmcdev=0

mmcpart=1

mmcroot=/dev/mmcblk0p2 rootwait rw

netargs=setenv bootargs console=${console},${baudrate} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp

netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${image}; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if ${get_cmd} ${fdt_addr} ${fdt_file}; then bootz ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;

panel=TFT43AB

script=boot.scr

 

Environment size: 2415/8188 bytes

=> mmc list

FSL_SDHC: 0 (SD)

FSL_SDHC: 1

=> mmc part

Partition Map for MMC device 0  --   Partition Type: DOS

 

Part    Start Sector    Num Sectors     UUID            Type

  1     8192            16384           0aad0b47-01     0c

  2     24576           1949696         0aad0b47-02     83

=> mmc dev

switch to partitions #0, OK

mmc0 is current device

=>boot

usbcore: registered new interface driver ath3k

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci-pltfm: SDHCI platform and OF driver helper

/soc/aips-bus@02100000/usdhc@02190000: voltage-ranges unspecified

sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO

sdhci-esdhc-imx 2190000.usdhc: No vqmmc regulator found

mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA

/soc/aips-bus@02100000/usdhc@02194000: voltage-ranges unspecified

sdhci-esdhc-imx 2194000.usdhc: could not get ultra high speed state, work on normal mode

sdhci-esdhc-imx 2194000.usdhc: No vmmc regulator found

sdhci-esdhc-imx 2194000.usdhc: No vqmmc regulator found

mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA

caam 2140000.caam: Entropy delay = 3200

caam 2140000.caam: Instantiated RNG4 SH0

mmc1: MAN_BKOPS_EN bit is not set

caam 2140000.caam: Instantiated RNG4 SH1

caam 2140000.caam: device ID = 0x0a16030000000000 (Era -524)

caam 2140000.caam: job rings = 3, qi = 0

mmc1: new DDR MMC card at address 0001

mmcblk1: mmc1:0001 P1XXXX 7.20 GiB

mmcblk1boot0: mmc1:0001 P1XXXX partition 1 16.0 MiB

mmcblk1boot1: mmc1:0001 P1XXXX partition 2 16.0 MiB

mmcblk1rpmb: mmc1:0001 P1XXXX partition 3 128 KiB

caam algorithms registered in /proc/crypto

caam_jr 2141000.jr0: registering rng-caam

can-3v3: disabling

ALSA device list:

  No soundcards found.

Waiting for root device /dev/mmcblk0p2...

#then it is stuck

 

 

P.S.below is what I modified for uboot. or else imx-uboot can't find card to load zimage.

Uboot Change 1:

 /home/dev/IMX/fsl-release-bsp/build_imx6ulevk/tmp/work/imx6ulevk-poky-linux-gnueabi/u-boot-imx/2016.03-r0/git/board/freescale/mx6ul_14x14_evk/ mx6ul_14x14_evk.c

//EVK original code:

int board_mmc_getcd(struct mmc *mmc)

{

        struct fsl_esdhc_cfg *cfg = (struct fsl_esdhc_cfg *)mmc->priv;

        int ret = 0;

 

        switch (cfg->esdhc_base) {

        case USDHC1_BASE_ADDR:

                ret = !gpio_get_value(USDHC1_CD_GPIO);

                break;

        case USDHC2_BASE_ADDR:

#if defined(CONFIG_MX6UL_EVK_EMMC_REWORK)

                ret = 1;

#else

                imx_iomux_v3_setup_multiple_pads(usdhc2_cd_pads,

                                                 ARRAY_SIZE(usdhc2_cd_pads));

                gpio_direction_input(USDHC2_CD_GPIO);

 

                /*

                 * Since it is the DAT3 pin, this pin is pulled to

                 * low voltage if no card

                 */

                ret = gpio_get_value(USDHC2_CD_GPIO);

 

                imx_iomux_v3_setup_multiple_pads(usdhc2_dat3_pads,

                                                 ARRAY_SIZE(usdhc2_dat3_pads));

#endif

                break;

        }

 

        return ret;

}

//modified code

int board_mmc_getcd(struct mmc *mmc)

{

        struct fsl_esdhc_cfg *cfg = (struct fsl_esdhc_cfg *)mmc->priv;

        int ret = 0;

 

        switch (cfg->esdhc_base) {

        case USDHC1_BASE_ADDR:

                ret = 1; //manually ensure that card is in slot

                break;

        case USDHC2_BASE_ADDR:

#if defined(CONFIG_MX6UL_EVK_EMMC_REWORK)

                ret = 1;

#else

                imx_iomux_v3_setup_multiple_pads(usdhc2_cd_pads,

                                                 ARRAY_SIZE(usdhc2_cd_pads));

                gpio_direction_input(USDHC2_CD_GPIO);

 

                /*

                 * Since it is the DAT3 pin, this pin is pulled to

                 * low voltage if no card

                 */

                ret = gpio_get_value(USDHC2_CD_GPIO);

 

                imx_iomux_v3_setup_multiple_pads(usdhc2_dat3_pads,

                                                 ARRAY_SIZE(usdhc2_dat3_pads));

#endif

                break;

        }

 

        return ret;

}

Uboot Change 2:

diff include/configs/mx6ul_14x14_evk.h.old include/configs/mx6ul_14x14_evk.h

67c67

< #define CONFIG_SYS_FSL_ESDHC_ADDR     USDHC2_BASE_ADDR

---

> #define CONFIG_SYS_FSL_ESDHC_ADDR     USDHC1_BASE_ADDR

 

Labels (3)
1 Solution
5,803 Views
listplot3d
Contributor III

problem solved. extra change on device tree is needed, working one as shown below:

emacs /home/dev/IMX/fsl-release-bsp/build_imx6ulevk/tmp/work/imx6ulevk-poky-linux-gnueabi/linux-imx/4.1.15-r0/git/arch/arm/boot/dts/imx6ul-14x14-evk.dts

/*  
&usdhc1 {
pinctrl-names = "default", "state_100mhz", "state_200mhz";
pinctrl-0 = <&pinctrl_usdhc1>;
pinctrl-1 = <&pinctrl_usdhc1_100mhz>;
pinctrl-2 = <&pinctrl_usdhc1_200mhz>;
cd-gpios = <&gpio1 19 GPIO_ACTIVE_LOW>;
keep-power-in-suspend;
enable-sdio-wakeup;
vmmc-supply = <&reg_sd1_vmmc>;
status = "okay";
};
*/

&usdhc1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_usdhc1>;
non-removable;
status = "okay";
};

&usdhc2 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_usdhc2>;
/* non-removable; */
status = "okay";
};

View solution in original post

11 Replies
5,804 Views
GregDyess
Contributor III

Did you also update /etc/fstab?

0 Kudos
5,804 Views
listplot3d
Contributor III

I didn't change /etc/fstab

0 Kudos
5,804 Views
srikanthmediset
Contributor I

Hi Li,

    I am trying to boot EVK custom board of DRAM 512 MB. I compiled the source with some changes but the board was hanging as shown below:

U-Boot 2014.04-08637-gaffa03210f-dirty (Aug 11 2017 - 15:40:06)

CPU: Freescale i.MX6SL rev1.2 at 792 MHz
CPU: Temperature 39 C, calibration data: 0x59a51269
Reset cause: POR
Board: MX6SLEVK
I2C: ready
DRAM:

   I am using Android 4.4.3 source and flashing images into eMMC. I tried with your changes also as mentioned in the above post but was helpless.Can you suggest me anything to overcome this one.

Regards,

srikanth.

0 Kudos
5,804 Views
listplot3d
Contributor III

looks like problem happened while detection DRAM. as UART is ok already, here is a slow but feasible method: you can add some debug in uboot source code to see what's going on.

0 Kudos
5,804 Views
Yuri
NXP Employee
NXP Employee

Hello,

  On the EVK (with demo image) it is enough to change U-boot environment  :

mmcdev=0

mmcroot=/dev/mmcblk0p2 rootwait rw

 

and system boots from SD port 0.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
5,804 Views
listplot3d
Contributor III

Hi Yuri,

  thanks for your reply. But that setting doesn't work:

-------------------------

=> echo $mmcdev
0
=> echo $mmcroot
/dev/mmcblk0p2 rootwait rw
=> boot
MMC: no card present
MMC: no card present
MMC: no card present
Booting from net ...
*** ERROR: `ethaddr' not set
*** ERROR: `ethaddr' not set
Bad Linux ARM zImage magic!
=>

---------------------------

this is why I changed uboot.

Thanks & Best Regards

-Shawn

0 Kudos
5,804 Views
listplot3d
Contributor III

Hi Yuri,

  below is the uboot output of the demo image from your first link.

----------------

U-Boot 2016.03-imx_v2016.03_4.1.15_2.0.0_ga+g0ec2a01 (Nov 11 2016 - 03:51:17 -0600)

CPU: Freescale i.MX6UL rev1.1 528 MHz (running at 396 MHz)
CPU: Industrial temperature grade (-40C to 105C) at 30C
Reset cause: POR
Board: MX6UL 14x14 EVK
I2C: ready
DRAM: 512 MiB
force_idle_bus: sda=0 scl=0 sda.gp=0x1d scl.gp=0x1c
force_idle_bus: failed to clear bus, sda=0 scl=1
MMC: FSL_SDHC: 0, FSL_SDHC: 1
MMC: no card present
*** Warning - MMC init failed, using default environment

Display: TFT43AB (480x272)
Video: 480x272x24
In: serial
Out: serial
Err: serial
MMC: no card present
Net: Board Net Initialization Failed
No ethernet found.
Normal Boot
Hit any key to stop autoboot: 0
MMC: no card present
MMC: no card present
MMC: no card present
Booting from net ...
No ethernet found.
No ethernet found.
Bad Linux ARM zImage magic!

=> mmc list
FSL_SDHC: 0
FSL_SDHC: 1
=> mmc part
MMC: no card present
=>

=> setenv mmcroot /dev/mmcblk0p2 rootwait rw
=> setenv mmcdev 0
=> boot
MMC: no card present
MMC: no card present
MMC: no card present
Booting from net ...
No ethernet found.
No ethernet found.
Bad Linux ARM zImage magic!
=>

---------------

My analysis and what has been done:

  with dip switch config, my board is booted from FSL_SDHC_0, then uboot loaded. this means hardware should be alright. I searched the string "MMC: no card present" in uboot source code, then found the reason it gets there is because uboot was trying card detection but failed. so I 'muted' the card detection logic in uboot and always return true over there, as shown in my first post of this thread. Now uboot can load zimage successfully and enter kernel boot.

However, there is another problem followed in kernel boot -- system locked at "Waiting for root device /dev/mmcblk0p2..." this is where I am stucking at.

Thanks & Regards

-Shawn

0 Kudos
5,804 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Please check SD1_CD pin.

https://community.nxp.com/thread/453954 

Regards,

Yuri.

0 Kudos
5,804 Views
listplot3d
Contributor III

problem solved. extra change on device tree is needed, working one as shown below:

emacs /home/dev/IMX/fsl-release-bsp/build_imx6ulevk/tmp/work/imx6ulevk-poky-linux-gnueabi/linux-imx/4.1.15-r0/git/arch/arm/boot/dts/imx6ul-14x14-evk.dts

/*  
&usdhc1 {
pinctrl-names = "default", "state_100mhz", "state_200mhz";
pinctrl-0 = <&pinctrl_usdhc1>;
pinctrl-1 = <&pinctrl_usdhc1_100mhz>;
pinctrl-2 = <&pinctrl_usdhc1_200mhz>;
cd-gpios = <&gpio1 19 GPIO_ACTIVE_LOW>;
keep-power-in-suspend;
enable-sdio-wakeup;
vmmc-supply = <&reg_sd1_vmmc>;
status = "okay";
};
*/

&usdhc1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_usdhc1>;
non-removable;
status = "okay";
};

&usdhc2 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_usdhc2>;
/* non-removable; */
status = "okay";
};

5,804 Views
listplot3d
Contributor III

I tried L4.1.15_2.0.0-ga_images_MX6UL7D.tar.gz, but as the link you mentioned is updated version, let me have a try again.

Thanks & Regards

-Shawn

0 Kudos