custom splash screen - i.mx6ull yocto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

custom splash screen - i.mx6ull yocto

1,386 Views
rob_lepage
Contributor I

My goal is to have a custom splash screen displayed from power up through my application's start.

I'm using an i.mx6ULL with a Phytec Yocto Vendor distribution (BSP-Yocto-Vendor-phyBOARD-Segin-PD17.1.2) with a 3x5 lcd display.  I've been searching, and believe I need to modified the psplash recipe, but have not had any success.

Please point me at available documentation, or give instruction on how to show my custom splash screen.

Thanks,

-Rob 

Labels (1)
1 Reply

1,148 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rob

one can look on

Patch to support uboot logo keep from uboot to kernel for NXP Linux and Android BSP (HDMI, LCD and L... 

GitHub - g0hl1n/psplash: Very simple boot splash screen - forked from: http://git.yoctoproject.org/g... 

https://community.nxp.com/thread/456343 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------