custom license in bb file of yocto

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

custom license in bb file of yocto

ソリューションへジャンプ
15,270件の閲覧回数
michaelma
Contributor I

I made a recipe "myrecipe.bb" in Yocto, and I add "LICENSE=commercial" in it.

Can i use "commercial" ? or I must use one of these : GPL, MIT, BSD, balabalabala

When I use "LICENSE=commercial", a warning happen when I did "bitbake myrecipe"

"

The license listed commercial was not in the licenses collected for recipe myrecipe

"

how to resolve the warning?

anybody knows?

タグ(1)
0 件の賞賛
返信
1 解決策
13,864件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello  Michael Ma,

Bitbake will look for the full license document of the license you have selected. It would seem that it has not found the license that corresponds to “commercial”. You may use any license you want as sometimes you need a very specific license for certain packages, but you must provide with the license text to resolve this warning.

You can add the license and the path, which would look something like:

LICENSE_PATH += "${LAYERDIR}/custom-licenses"

This inside your layer.conf file.

I hope this helps!

Regards,

元の投稿で解決策を見る

2 返答(返信)
13,865件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello  Michael Ma,

Bitbake will look for the full license document of the license you have selected. It would seem that it has not found the license that corresponds to “commercial”. You may use any license you want as sometimes you need a very specific license for certain packages, but you must provide with the license text to resolve this warning.

You can add the license and the path, which would look something like:

LICENSE_PATH += "${LAYERDIR}/custom-licenses"

This inside your layer.conf file.

I hope this helps!

Regards,

13,864件の閲覧回数
michaelma
Contributor I

Thank you for your answer.

I tried your suggestion to add LICENSE_PATH += "${LAYERDIR}/custom-licenses" which contains file "commercial".

  1. Firstly, I run "bitbake core-image-my" which contains my recipe "myrecipe".This warning is still there.
  2. Secondly, I run "bitbake -c clean myrecipe && bitbake -c cleansstate myrecipe", and then "bitbake core-image-my".This warning is gone.

So, I feel that, although adding LICENSE_PATH += "${LAYERDIR}/custom-licenses" , we should clean recipes firstly.

After that, the effect of LICENSE_PATH += "${LAYERDIR}/custom-licenses" will work.

Thank you again, nice answer :smileyhappy:

0 件の賞賛
返信