custom board emmc error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

custom board emmc error

1,088 次查看
yufe
Contributor II

my custom board is based on sabresd board. use mfg tools to download firmware, and have errors when mfg linux write file to emmc.

my bsp version is L3.14.52. dcd table is updated by ddr tester. 

some console output is below, detail output is attached.

 

UTP: received command '$ echo 0 > /sys/block/mmcblk3boot0/force_ro'

UTP: executing "echo 0 > /sys/block/mmcblk3boot0/force_ro"

sh: /sys/block/mmcblk3boot0/force_ro: No such file or directory

UTP: sending Non-success to kernel for command $ echo 0 > /sys/block/mmcblk3boot0/force_ro.

mmc3: error -110 whilst initialising MMC card utp_poll: exit with status 256

mmc3: error -110 whilst initialising MMC card

mmc3: error -110 whilst initialising MMC card

mmc3: error -110 whilst initialising MMC card

 

-------

add something about u-boot emmc result:

i use mfg tool to load u-boot only, and in u-boot cmd, type "mmc list" or "mmc dev 2" cmd, i got no vaild message. but when i change board the .cfg file from mx6qp.cfg to mx6q_4x_mt41j128.cfg, "mmc dev 2" cmd output some emmc info, although it's not correct info because the bus-width is 1 and capacity is 1k: . so i think something is wrong in dcd cfg file.

i modify mx6qp.cfg as this:run I.MX6DQSDL DDR3 Script Aid V0.10.xlsx, get an .inc file, and then use DDR_Tester.exe to test it, chage the leveling calibration,DQS Gating,Read&Write calibration to mx6qp.cfg file. there are many differences between .inc file and .cfg file, is it right only modify part of them?

Original Attachment has been moved to: output.txt.zip

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

694 次查看
igorpadykov
NXP Employee
NXP Employee

Hi yu

please look at similar issue on https://freescale.jiveon.com/thread/320449
so please try to rebuild mfg tools firmware for custom board using
sect.6.2 Manufacturing Tool, MFGTool attached Yocto Guide

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复