cpuburn-neon-20140626-r0 do_fetch: Fetcher failure for i.mx6ul (L4.14.98)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

cpuburn-neon-20140626-r0 do_fetch: Fetcher failure for i.mx6ul (L4.14.98)

794 次查看
824497590
Contributor I

824497590_0-1611540073472.png

My network is OK, but every time I download the cpuburn-neon-20140626-r0 file, it fails. What else do I need to do to download this file

 

0 项奖励
回复
2 回复数

789 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hi ,

Attachment is files of cpuburn-neon-20140626. 

1. decompress it at first on windows.

weidong_sun_0-1611545980726.png

 

2. copy it to downloads

Enter into ubuntu:

# cd fsl-yocto-bsp/downloads

# mkdir cpuburn-neon-20140626

then copy above 4 files to the directory.

 

This means when you begin to compile image again, cpuburn-neon will not be downloaded .

Try it, please!

 

Hope it can help to you.

Have a nice day!

B.R,

Weidong

712 次查看
小李
Contributor III
0 项奖励
回复