could IMX6Solo support DDR3-1600?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

could IMX6Solo support DDR3-1600?

ソリューションへジャンプ
1,273件の閲覧回数
haiboyang
Contributor I

Hello,sir

i notice  IMX6Solo could support DDR3-800, but not sure if it could support DDR3-1600, could you please help confirm? thanks.

 

haibo

ラベル(1)
0 件の賞賛
返信
1 解決策
1,200件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello

  i.MX6 S/DL support DDR3/DDR3L/LPDDR2-800 ; maximum DRAM frequency

is 400 MHz. Therefore the "more speedy" DRAM parts, should be configured for

400 MHz (800).

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,201件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello

  i.MX6 S/DL support DDR3/DDR3L/LPDDR2-800 ; maximum DRAM frequency

is 400 MHz. Therefore the "more speedy" DRAM parts, should be configured for

400 MHz (800).

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------