could IMX6Solo support DDR3-1600?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

could IMX6Solo support DDR3-1600?

Jump to solution
1,262 Views
haiboyang
Contributor I

Hello,sir

i notice  IMX6Solo could support DDR3-800, but not sure if it could support DDR3-1600, could you please help confirm? thanks.

 

haibo

Labels (1)
0 Kudos
Reply
1 Solution
1,189 Views
Yuri
NXP Employee
NXP Employee

Hello

  i.MX6 S/DL support DDR3/DDR3L/LPDDR2-800 ; maximum DRAM frequency

is 400 MHz. Therefore the "more speedy" DRAM parts, should be configured for

400 MHz (800).

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,190 Views
Yuri
NXP Employee
NXP Employee

Hello

  i.MX6 S/DL support DDR3/DDR3L/LPDDR2-800 ; maximum DRAM frequency

is 400 MHz. Therefore the "more speedy" DRAM parts, should be configured for

400 MHz (800).

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------