1.
Please check if the demo image is working on Your board.
To prepare SD card image :
$ sudo dd if=core-image-minimal-dev-imx53qsb.sdcard of=/dev/sdb bs=1M
http://downloads.yoctoproject.org/releases/yocto/yocto-1.6/machines/imx53qsb/core-image-minimal-dev-...
Please look at the following for some details.
"Task #4 - Deploy and test"
https://community.freescale.com/docs/DOC-94989
2.
As for host PC configuring, please refer to sections 6.1 (Setup Terminal) and
3.2 (How to Boot From Micro SD Card) of the enclosed "i.MX53_START_Linux_BSP_UserGuide.pdf"
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------