I have a i.MX6 board with display connected over LVDS. I got the following command running to get video streaming over IP using gstreamer-0.10
On IMX6
gst-launch -v udpsrc port=5004 ! application/x-rtp, payload=96 ! rtph264depay ! vpudec low-latency=true ! imxv4l2sink sync=false
On my PC:
C:\gstreamer\1.0\x86_64\bin\gst-launch-1.0.exe -v filesrc location=C:\\gstreamer\\1.0\\x86_64\\bin\\hash.h264 ! h264parse ! rtph264pay ! udpsink host=153.77.205.139 port=5004 sync=true
But when I shifted to gstreamer-1.0 , i am facing the issue, it is failing when I am trying to stream:
gst-launch-1.0 -v udpsrc port=5004 ! application/x-rtp, payload=96 ! rtph264 depay ! imxvpudec ! imxipuvideosink sync=false
Can you please help in converting gstreamer-0.10 pipeline to gstreamer-1.0