connection fail to git server..

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

connection fail to git server..

1,390 次查看
seyoungkim
Contributor II

Hi everyone.

in a yocto repo download step making error

->>>  git://git.freescale.com/imx/linux-imx.git.  and u-boot-imx  too..

it makes error message "connection refusd."

i tried change network access-point to my phone. but it makes same error.

标记 (1)
0 项奖励
回复
2 回复数

1,233 次查看
igorpadykov
NXP Employee
NXP Employee

Hi seyoung

please look at

[meta-freescale] Issue with freescale git server at git.freescale.com 

[meta-freescale] [PATCH] linux-imx: Change git repository URL 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,233 次查看
rensdol
Contributor I

Is someone working on this?  I have this error trying to build the manufacturing tools for imx7dsabresd.

ERROR: u-boot-imx-mfgtool-2016.03-r0 do_fetch: Fetcher failure: Fetch command failed with exit code 128, output:
Cloning into bare repository '/home/rens/yocto/fsl-release-bsp/downloads//git2/git.freescale.com.imx.uboot-imx.git'...
fatal: read error: Connection reset by peer.

Sorry wrong error this was a local network error,  

The build is stuck at

Currently 2 running tasks (1471 of 1538):
0: linux-imx-4.1.15-r0 do_fetch (pid 2733)
1: mfgtool-linux-imx-4.1.15-r0 do_fetch (pid 2734)

Is there a dedicated forum thread for git server status and error reports?

Regards

Rens

0 项奖励
回复