configure cpu frequency to 800MHz for MC IMX6USEVM10AB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

configure cpu frequency to 800MHz for MC IMX6USEVM10AB

1,129件の閲覧回数
shreeharsha_ind
Contributor II

Hi All,

Kindly help us configuring CPU frequency to 800MHZ in kernel for MC IMX6USEVM10AB. However currently we see the frequency value to be at 1GHz.

Regards,

Shree

0 件の賞賛
返信
3 返答(返信)

1,102件の閲覧回数
shreeharsha_ind
Contributor II

Hi Team,

We would like to understand the impacts on Power and Thermal qualifcation which has been carried out with old part numbers running at 800mhz.

Please let us know the impact if we change IMX6 chip running at 800Mhz to 1Ghz part number. What all areas are impacted for a PCB layout such as DDR , Power, Thermal ,etc.

Kindly share the update at earliest.



Regards,

Shree

0 件の賞賛
返信

1,112件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Shree

 

one can try to adjust  cpu0: cpu@0 {..
operating-points =

in dts:

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6dl.dtsi?h=imx_5.4.70...

use Table 8. Operating Ranges   i.MX 6Solo/6DualLite Applications Processors for Consumer Products

 

Best regards
igor

0 件の賞賛
返信

1,119件の閲覧回数
sureshrao
NXP Employee
NXP Employee

Hello @shreeharsha_ind ,

Please check Section 2.5.3 CPU frequency scaling of Linux Reference manual for configuring frequency of operation.  The Linux documentation bundle can be downloaded from below link

https://www.nxp.com/webapp/Download?colCode=L4.14.98_2.3.0_LINUX_DOCS

 

Best Regards,

Suresh

0 件の賞賛
返信