configure cpu frequency to 800MHz for MC IMX6USEVM10AB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

configure cpu frequency to 800MHz for MC IMX6USEVM10AB

1,077 Views
shreeharsha_ind
Contributor II

Hi All,

Kindly help us configuring CPU frequency to 800MHZ in kernel for MC IMX6USEVM10AB. However currently we see the frequency value to be at 1GHz.

Regards,

Shree

0 Kudos
Reply
3 Replies

1,050 Views
shreeharsha_ind
Contributor II

Hi Team,

We would like to understand the impacts on Power and Thermal qualifcation which has been carried out with old part numbers running at 800mhz.

Please let us know the impact if we change IMX6 chip running at 800Mhz to 1Ghz part number. What all areas are impacted for a PCB layout such as DDR , Power, Thermal ,etc.

Kindly share the update at earliest.



Regards,

Shree

0 Kudos
Reply

1,060 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shree

 

one can try to adjust  cpu0: cpu@0 {..
operating-points =

in dts:

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6dl.dtsi?h=imx_5.4.70...

use Table 8. Operating Ranges   i.MX 6Solo/6DualLite Applications Processors for Consumer Products

 

Best regards
igor

0 Kudos
Reply

1,067 Views
sureshrao
NXP Employee
NXP Employee

Hello @shreeharsha_ind ,

Please check Section 2.5.3 CPU frequency scaling of Linux Reference manual for configuring frequency of operation.  The Linux documentation bundle can be downloaded from below link

https://www.nxp.com/webapp/Download?colCode=L4.14.98_2.3.0_LINUX_DOCS

 

Best Regards,

Suresh

0 Kudos
Reply