config file is not updating after doing menuconfig

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

config file is not updating after doing menuconfig

跳至解决方案
7,183 次查看
chandraevolute
Contributor V

I am having imx6ulevk board using this git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.14.38-6UL_ga repo.

I am doing bitbake -c menuconfig linux-imx, I am disabling LCD, Video, FB and Sound drivers, Keybaord . when I check the .config file still these are set to "y". these are some of the configs. Why this is happening.

CONFIG_KEYBOARD_GPIO=y

CONFIG_KEYBOARD_SNVS_PWRKEY=y

CONFIG_KEYBOARD_IMX=y

CONFIG_MOUSE_PS2=m

CONFIG_MOUSE_PS2_ELANTECH=y

CONFIG_FB=y

CONFIG_FB_MXS=y

CONFIG_BACKLIGHT_LCD_SUPPORT=y

CONFIG_LCD_CLASS_DEVICE=y

CONFIG_LCD_L4F00242T03=y

CONFIG_LCD_PLATFORM=y

CONFIG_BACKLIGHT_CLASS_DEVICE=y

CONFIG_BACKLIGHT_PWM=y

CONFIG_FB_MXC_SYNC_PANEL=y

CONFIG_FB_MXC_LDB=y

CONFIG_FB_MXC_MIPI_DSI_SAMSUNG=y

CONFIG_FB_MXC_TRULY_WVGA_SYNC_PANEL=y

CONFIG_FB_MXC_HDMI=y

CONFIG_FB_MXC_EINK_PANEL=y

CONFIG_FB_MXC_EINK_V2_PANEL=y

CONFIG_FB_MXS_SII902X=y

And also when i try top copy this config file ../sources there is no linux-imx -3.14.38 instead i have 3.14.28 sources and bb files. you an see the list of files below present.

drwxrwxrwx 3 root root 4096 Jun 12 22:35 linux-fslc

-rwxrwxrwx 1 root root  681 Jun 12 22:35 linux-fslc_4.1.bb

-rwxrwxrwx 1 root root  370 Jun 12 22:35 linux-fslc.inc

drwxrwxrwx 2 root root 4096 Jun 12 22:35 linux-imx

drwxrwxrwx 5 root root 4096 Jun 12 22:35 linux-imx-2.6.35.3

-rwxrwxrwx 1 root root  908 Jun 12 22:35 linux-imx_2.6.35.3.bb

drwxrwxrwx 3 root root 4096 Jun 12 22:35 linux-imx-3.14.28

-rwxrwxrwx 1 root root  993 Jun 12 22:35 linux-imx_3.14.28.bb

-rwxrwxrwx 1 root root  665 Jun 12 22:35 linux-imx.inc

drwxrwxrwx 3 root root 4096 Jun 12 22:35 linux-imx-mfgtool-3.14.28

-rwxrwxrwx 1 root root  380 Jun 12 22:35 linux-imx-mfgtool_3.14.28.bb

drwxrwxrwx 3 root root 4096 Jun 12 22:35 linux-imx-rt-3.14.28

-rwxrwxrwx 1 root root 1241 Jun 12 22:35 linux-imx-rt_3.14.28.bb

drwxrwxrwx 2 root root 4096 Jun 12 22:35 linux-ls1

-rwxrwxrwx 1 root root  364 Jun 12 22:35 linux-ls1_3.12.bb

-rwxrwxrwx 1 root root  780 Jun 12 22:35 linux-ls1.inc

-rwxrwxrwx 1 root root 3000 Jun 12 22:35 linux-mfgtool.inc

drwxrwxrwx 2 root root 4096 Jun 12 22:35 linux-timesys-3.0.15

-rwxrwxrwx 1 root root  719 Jun 12 22:35 linux-timesys_3.0.15.bb

linux@ubuntu:/home/fsl-release-bsp/sources/meta-fsl-arm/recipes-k

Edit 1 :

I found that linux-imx -3.14.38.bb is present in meta-fsl-bsp-release/imx/meta-bsp

below is my bb layer conf

LCONF_VERSION = "6"

BBPATH = "${TOPDIR}"

BSPDIR := "${@os.path.abspath(os.path.dirname(d.getVar('FILE', True)) + '/../..')}"

BBFILES ?= ""

BBLAYERS = " \

  ${BSPDIR}/sources/poky/meta \

  ${BSPDIR}/sources/poky/meta-yocto \

  \

  ${BSPDIR}/sources/meta-openembedded/meta-oe \

  ${BSPDIR}/sources/meta-openembedded/meta-multimedia \

  \

  ${BSPDIR}/sources/meta-fsl-arm \

  ${BSPDIR}/sources/meta-fsl-arm-extra \

  ${BSPDIR}/sources/meta-fsl-demos \

"

##Freescale Yocto Release layer

BBLAYERS += " ${BSPDIR}/sources/meta-fsl-bsp-release/imx/meta-bsp "

BBLAYERS += " ${BSPDIR}/sources/meta-fsl-bsp-release/imx/meta-sdk "

BBLAYERS += " ${BSPDIR}/sources/meta-browser "

BBLAYERS += " ${BSPDIR}/sources/meta-openembedded/meta-gnome "

BBLAYERS += " ${BSPDIR}/sources/meta-openembedded/meta-networking "

BBLAYERS += " ${BSPDIR}/sources/meta-openembedded/meta-python "

BBLAYERS += " ${BSPDIR}/sources/meta-openembedded/meta-ruby "

BBLAYERS += " ${BSPDIR}/sources/meta-openembedded/meta-filesystems "

BBLAYERS += " ${BSPDIR}/sources/meta-qt5 "

When I do bitbake linu-imx th .sdcard image is showing aroung 880 MB... Is it common?

标签 (2)
0 项奖励
回复
1 解答
6,542 次查看
saurabh206
Senior Contributor III

bitbake linux-imx -c menuconfig

You can copy .config to my_custom_deficonf

linux-imx_3.14.38.bb

do_configure_prepend() {

   cp ${S}/arch/arm/configs/my_custom_deficonf  ${S}/.config

   cp ${S}/arch/arm/configs/my_custom_deficonf  ${S}/../defconfig

}

在原帖中查看解决方案

0 项奖励
回复
9 回复数
6,542 次查看
chandraevolute
Contributor V

Will try these commands SaurabhPatel​ and let you know the result

Thanks

0 项奖励
回复
6,543 次查看
saurabh206
Senior Contributor III

bitbake linux-imx -c menuconfig

You can copy .config to my_custom_deficonf

linux-imx_3.14.38.bb

do_configure_prepend() {

   cp ${S}/arch/arm/configs/my_custom_deficonf  ${S}/.config

   cp ${S}/arch/arm/configs/my_custom_deficonf  ${S}/../defconfig

}

0 项奖励
回复
6,542 次查看
chandraevolute
Contributor V

If I try to build freshly by removing the previous build directory I am getting below errors

linux@ubuntu:/home/fsl-release-bsp/FreshBuild$ bitbake fsl-image-gui

Parsing recipes: 100% |#################################################################################################################################| Time: 00:01:34

Parsing of 2049 .bb files complete (0 cached, 2049 parsed). 2564 targets, 157 skipped, 0 masked, 0 errors.

NOTE: Resolving any missing task queue dependencies

NOTE: multiple providers are available for jpeg (jpeg, libjpeg-turbo)

NOTE: consider defining a PREFERRED_PROVIDER entry to match jpeg

NOTE: multiple providers are available for jpeg-native (jpeg-native, libjpeg-turbo-native)

NOTE: consider defining a PREFERRED_PROVIDER entry to match jpeg-native

ERROR: Nothing PROVIDES 'virtual/libgles2' (but /home/fsl-release-bsp/sources/poky/meta/recipes-multimedia/gstreamer/gstreamer1.0-plugins-bad_1.4.5.bb, /home/fsl-release-bsp/sources/poky/meta/recipes-graphics/mesa/mesa-demos_8.2.0.bb DEPENDS on or otherwise requires it)

ERROR: amd-gpu-x11-bin-mx51 PROVIDES virtual/libgles2 but was skipped: incompatible with machine imx6ulevk (not in COMPATIBLE_MACHINE)

ERROR: amd-gpu-bin-mx51 PROVIDES virtual/libgles2 but was skipped: incompatible with machine imx6ulevk (not in COMPATIBLE_MACHINE)

NOTE: Runtime target 'gstreamer1.0-plugins-bad-meta' is unbuildable, removing...

Missing or unbuildable dependency chain was: ['gstreamer1.0-plugins-bad-meta', 'virtual/libgles2']

NOTE: Runtime target 'packagegroup-fsl-multimedia-gstreamer1.0-core' is unbuildable, removing...

Missing or unbuildable dependency chain was: ['packagegroup-fsl-multimedia-gstreamer1.0-core', 'gstreamer1.0-plugins-bad-meta', 'virtual/libgles2']

ERROR: Required build target 'fsl-image-gui' has no buildable providers.

Missing or unbuildable dependency chain was: ['fsl-image-gui', 'packagegroup-fsl-multimedia-gstreamer1.0-core', 'gstreamer1.0-plugins-bad-meta', 'virtual/libgles2']

Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

0 项奖励
回复
6,542 次查看
saurabh206
Senior Contributor III

You can run following command sequences

bitbake -f -c clean <package_name>

bitbake -f -c compile <package_name>

0 项奖励
回复
6,542 次查看
chandraevolute
Contributor V

Hi saurabh206​ i downloaded the fresh package.

Now i am able to compile the kernel.

But still when i do bitbake linu-imx -c menuconfig i am unable to generate the modifed image. config file is not chnaging.

0 项奖励
回复
6,542 次查看
chandraevolute
Contributor V

Hi saurabh206​thank you

I followed the below steps

1. bitbake linux-imx -c menuconfig

2. After doing menuconfig copy the .conig to ../defconfig

3. later copy that .config to (build_dir)/work-shared/imx6ulevk/kernel-source/arch/arm/configs/imx_v7_defconfig and imx_v6_v7_defconfig.

it worked

0 项奖励
回复
6,542 次查看
saurabh206
Senior Contributor III

Good You are able to solve your issue.

0 项奖励
回复
6,542 次查看
chandraevolute
Contributor V

again I am getting the same error

linux@ubuntu:/home/fsl-release-bsp/FreshBuild$ bitbake -f -c clean fsl-image-gui

Loading cache: 100% |###################################################################################################################################| ETA:  00:00:00

Loaded 2565 entries from dependency cache.

NOTE: Resolving any missing task queue dependencies

NOTE: multiple providers are available for jpeg (jpeg, libjpeg-turbo)

NOTE: consider defining a PREFERRED_PROVIDER entry to match jpeg

NOTE: multiple providers are available for jpeg-native (jpeg-native, libjpeg-turbo-native)

NOTE: consider defining a PREFERRED_PROVIDER entry to match jpeg-native

ERROR: Nothing PROVIDES 'virtual/libgles2' (but /home/fsl-release-bsp/sources/poky/meta/recipes-multimedia/gstreamer/gstreamer1.0-plugins-bad_1.4.5.bb, /home/fsl-release-bsp/sources/poky/meta/recipes-graphics/mesa/mesa-demos_8.2.0.bb DEPENDS on or otherwise requires it)

ERROR: amd-gpu-bin-mx51 PROVIDES virtual/libgles2 but was skipped: incompatible with machine imx6ulevk (not in COMPATIBLE_MACHINE)

ERROR: amd-gpu-x11-bin-mx51 PROVIDES virtual/libgles2 but was skipped: incompatible with machine imx6ulevk (not in COMPATIBLE_MACHINE)

NOTE: Runtime target 'gstreamer1.0-plugins-bad-meta' is unbuildable, removing...

Missing or unbuildable dependency chain was: ['gstreamer1.0-plugins-bad-meta', 'virtual/libgles2']

NOTE: Runtime target 'packagegroup-fsl-multimedia-gstreamer1.0-core' is unbuildable, removing...

Missing or unbuildable dependency chain was: ['packagegroup-fsl-multimedia-gstreamer1.0-core', 'gstreamer1.0-plugins-bad-meta', 'virtual/libgles2']

ERROR: Required build target 'fsl-image-gui' has no buildable providers.

Missing or unbuildable dependency chain was: ['fsl-image-gui', 'packagegroup-fsl-multimedia-gstreamer1.0-core', 'gstreamer1.0-plugins-bad-meta', 'virtual/libgles2']

Tomorrow I am going to do a fresh copy of entire project and let you know the result by monday

0 项奖励
回复
6,542 次查看
chandraevolute
Contributor V

I checked the linux-imx_3.14.38.bb file and the lines were already added.

my question is why the changes are not reflecting in .config file.

When we do bitbake linux-imx -c menuconfig

the configuration is saved in .config file, but whatever i removed were also marked as "y" inside the .config file. 

0 项奖励
回复