communication between imx6 solo board to windows 7 pc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

communication between imx6 solo board to windows 7 pc

630 Views
srikittu34
Contributor II

i am trying to do ddr3 stress test tool there i have connected usb otg cable to board and windows 7 pc ..

it showing that it is unrecognised usb device..please someone suggest me how to doenload the usb otg drivers for imx6 board in windows 7   

Labels (2)
Tags (1)
0 Kudos
Reply
1 Reply

521 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Anna,
You could check on board’s user guide which USB port should be used. For example, on the SABRE-SD board, one of the OTG ports is a USB-UART for accessing to the debug serial port, while the other is connected to a USB controller of the i.MX processor, also having the Serial Downloader feature (properly configuring the boot switches).
In case of the SABRE-SD board, it uses the FT232 USB to serial bridge sold by FTDI chip. You could find the driver in the FTDI Chip website:

http://www.ftdichip.com/Drivers/VCP.htmhttp://www.ftdichip.com/Drivers/VCP.htm 


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------