Hello support team,
MACHINE=imx6qdlsabresd DISTRO=fsl-imx-wayland source ./imx-setup-release.sh -b build
bitbake imx-image-base
i have created the image based on the above configuration.
Now i want to run emulator for the above image/
i have given the command as runqemu imx6qdlsabresd. but its not working
whether can run emulator for imx6qdlsabresd? if it so can you suggest the command or documentation.
i.MX Yocto Project User's Guide, Rev. LF5.15.32_2.0.0 command to run emulator not given in this document.
thanks