coexistence of wifi and bluetooth.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

coexistence of wifi and bluetooth.

1,259 Views
mutyalaraoneela
Contributor III

Hi All,

Platform : imx6sl

Os : Android kitkat 4.4.3

     I made my module to run as wifi and bluetooth individually, but not I want to make it coexist. For that do I need to enable anything in the Android BSP????

Please suggest me how to proceed from here???

Thanks and Regards,

Mutyalarao.

0 Kudos
Reply
1 Reply

1,031 Views
igorpadykov
NXP Employee
NXP Employee

Hi mutyalarao

bluetooth and wifi stacks need to speak to each other to know when

is an appropriate time to prefer wifi traffic or bluetooth traffic and AR6103

has special signals called Bluetooth Coexistence Interface, however these signals

are not routed on connector on Sabre board.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply