clock signal of IMX6Q does not output SPI device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

clock signal of IMX6Q does not output SPI device

3,079件の閲覧回数
villager
Contributor II

Hello

 

I attached spi device to imx6q.

(spi dev was wired spi1)

 

pinmap is bellow

oled_sche.PNG

 

OLED_SCLK -----CSI0_DAT4

OLED_SDIN -----CSI0_DAT5

OLED_D_C/ -----CSI0_DAT6

OLED_CS/ -----CSI0_DAT7

 

CSI0_DAT4         ALT2     ECSPI1_SCLK

CSI0_DAT5         ALT      ECSPI1_MOSI

CSI0_DAT6         ALT      ECSPI1_MISO

CSI0_DAT7         ALT      ECSPI1_SS0

 

 oled_sche2.PNG

 

dts is bellow

 

           ecspi1: ecspi@02008000 {

               #address-cells = <1>;

               #size-cells = <0>;

               compatible = "fsl,imx6q-ecspi", "fsl,imx51-ecspi";

               reg = <0x02008000 0x4000>;

               interrupts = <0 31 IRQ_TYPE_LEVEL_HIGH>;

               clocks = <&clks IMX6QDL_CLK_ECSPI1>,

                   <&clks IMX6QDL_CLK_ECSPI1>;

               clock-names = "ipg", "per";

               dmas = <&sdma 3 7 1>, <&sdma 4 7 2>;

               dma-names = "rx", "tx";

               status = "disabled";

            };

 

&ecspi1 {

   fsl,spi-num-chipselects = <1>;

   cs-gpios = <&gpio5 25 0>;

   pinctrl-names = "default";

   pinctrl-0 = <&pinctrl_ecspi1>;

   /*status = "okay";*/

   status = "okay";

 

   spidev0: spi@0 {

      #address-cells = <1>;

      #size-cells = <1>;

      compatible = "spidev";

      reg = <0>;

      spi-max-frequency = <2000000>;

   };

 

pinctrl_ecspi1: ecspi1grp {

         fsl,pins = <

 

            MX6QDL_PAD_CSI0_DAT4__ECSPI1_SCLK   0x100b1

            MX6QDL_PAD_CSI0_DAT5__ECSPI1_MOSI   0x100b1

            MX6QDL_PAD_CSI0_DAT6__ECSPI1_MISO   0x100b1

            MX6QDL_PAD_CSI0_DAT7__ECSPI1_SS0    0x1b0b0

         >;

      }; 

but clock signal does not output.

does my dts wrong?

or do I need to set additional setting?

 

With best regards,

villager

0 件の賞賛
返信
5 返答(返信)

3,005件の閲覧回数
villager
Contributor II

HELLO @Yuri

 

my EVB is i.MX6Q, real target is i.MX6S/DL
There is not much difference between these two, so I wrote them in confusion.

The reason the clock does not tx is because there is no SPI clock setting.
According to the chip manual (IMX6SDLRM Rev. 1, 04/2013),
the PLL should be divided by /8 and /1.

villager_0-1645399430690.png

 

After booting, I set the following additional settings in linux application,

and the clock signal came out normally.

 

/* 2nd : change clock Register (CCM_CCOSR) */

    /* chip manual : 18.6.21 CCM Clock Output Source Register (CCM_CCOSR) */

 

    setting=0x0;

 

#define CLK01_SEL   ( 1<<3 | 0<<2 | 1<<1 | 1<<0) //1011 ahb_clk_root

#define CLK01_DIV   ( 1<<6 | 1<<5 | 1<<4) //111 divide by 8

#define CLK01_EN    ( 0<<7 )

#define CLK_OUT_SEL    ( 1<<8 )

#define CLK02_SEL   ( 0<<20 | 1<<19 | 1<<18 | 1<<17 | 0<<16)  //01110 osc_clk

#define CLK02_DIV   ( 0<<23 | 0<<22 | 0<<21) //111 divide by 8

#define CLK02_EN    ( 0<<24 )

 

    setting=(setting | CLK01_SEL);

    setting=(setting | CLK01_DIV);

    setting=(setting | CLK01_EN);

    setting=(setting | CLK_OUT_SEL);

    setting=(setting | CLK02_SEL);

    setting=(setting | CLK02_DIV);

    setting=(setting | CLK02_EN);

 

    read_reg=0;

    mmap_ioctl((unsigned long)&CCM_CCOSR, &read_reg, MMAP_RD);

 

    if(read_reg != setting)  {

        printf("@%p(CCM_CCOSR) change property 0x%x->0x%x\n"

                , (void *)&CCM_CCOSR, read_reg, setting);

        mmap_ioctl((unsigned long)&CCM_CCOSR, &setting, MMAP_WR);

 

    }

 

 

villager_1-1645399694169.png

 


thank you.

3,067件の閲覧回数
villager
Contributor II

hello igor,
thank you for your reply.

I already did spidev test and it didn't work properly,
so I took a check with an oscilloscope and found that the clock signal was not coming out.

 

best regards

villager

0 件の賞賛
返信

3,072件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Villager

 

one can look at testing procedure on below link

https://variwiki.com/index.php?title=VAR-SOM-MX6_Yocto_Unit_Testing_V7#SPI

 

Best regards
igor

0 件の賞賛
返信

3,054件の閲覧回数
villager
Contributor II

thank you igor.

I haven't made any progress yet.
I dumped the register.
can you please check if this value is correct?

 

//mux setting
@0x20e0080(IOMUXC_SW_MUX_CTL_PAD_CSI0_DATA07), read_reg 0x5
@0x20e0394(IOMUXC_SW_PAD_CTL_PAD_CSI0_DATA07), read_reg 0x1b0b0
@0x20e0074(IOMUXC_SW_MUX_CTL_PAD_CSI0_DATA04), read_reg 0x2
@0x20e0078(IOMUXC_SW_MUX_CTL_PAD_CSI0_DATA05), read_reg 0x2
@0x20e007c(IOMUXC_SW_MUX_CTL_PAD_CSI0_DATA06), read_reg 0x2
@0x20e0388(IOMUXC_SW_PAD_CTL_PAD_CSI0_DATA04), read_reg 0x100b1
@0x20e038c(IOMUXC_SW_PAD_CTL_PAD_CSI0_DATA05), read_reg 0x100b1
@0x20e0390(IOMUXC_SW_PAD_CTL_PAD_CSI0_DATA06), read_reg 0x100b1
//spi settng
@0x2008008(ECSPI1_CONREG), read_reg 0x7020f1
@0x200800c(ECSPI1_CONFIGREG), read_reg 0x100
//clock setting
@0x20c4060(CCM_CCOSR), read_reg 0xe017b

0 件の賞賛
返信

3,018件の閲覧回数
Yuri
NXP Employee
NXP Employee

@villager 
Hello,

   I looked at Your mux settings. As I see IOMUXC registers addresses do not correspond i.MX6Q.
They are for i.MX6S/DL.
  What is exact i.MX6  part  number on Your board?

Regards,
Yuri.

0 件の賞賛
返信