clko2 output problem on IMX8MQuad EVK board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

clko2 output problem on IMX8MQuad EVK board

1,163 Views
coindu
Contributor IV

Hi   All:

        how to use CLKO2 to ouput 24MHZ clock?

        in clk-imx8mq.c file can find CLKO2 parents input 

 

         static const char *imx8mq_clko2_sels[] = {"osc_25m", "sys2_pll_200m", "sys1_pll_400m", "sys2_pll_166m", "audio_pll1_out","video_pll1_out", "ckil", };

       

      when I use sys_pll_200m as clko2`s parent and set clock-rate to  24000000, the result mclk_clock will be 25M

 

pinctrl-0 = <&pinctrl_csi1>;
clocks = <&clk IMX8MQ_CLK_CLKO2_DIV>;
clock-names = "csi_mclk";
assigned-clocks = <&clk IMX8MQ_CLK_CLKO2_SRC>,
<&clk IMX8MQ_CLK_CLKO2_DIV>;
assigned-clock-parents = <&clk IMX8MQ_SYS2_PLL_200M>;
assigned-clock-rates = <0>, <24000000>;
csi_id = <0>;

 

      use sys_pill_166m as clko2`s parent ,  the result csi_mclk will be 23.8M

      

      please tell me show to ouput 24M precise with clko2

thanks

0 Kudos
Reply
2 Replies

1,051 Views
coindu
Contributor IV

Thanks a lot.  

0 Kudos
Reply

1,051 Views
igorpadykov
NXP Employee
NXP Employee

Hi coin

to ouput 24M precise with clko2 you should select appropriate parent clock

source which could be evenly (precisely) divided, probably reprogramming some plls.

For example sys_pill_166m can not be divided by some integer to get 24M, most close

divider 7 will give the result 23.8M.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply