chromium could not play video on network on imx93evk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

chromium could not play video on network on imx93evk

Jump to solution
1,308 Views
jiangyaqiang
Contributor V

Hi experts:

 

  I found that the chromium could not play video on network on platfrom imx93evk,

yocto: LF 6.1.55.  No log print out,  just show "network could not connect" on wed.

 Does any knows why ? 

 

  Thanks

 Best Regards

Labels (3)
Tags (1)
0 Kudos
Reply
1 Solution
1,210 Views
jiangyaqiang
Contributor V

HI Bio_TICFS:

 

Thanks .

I't's not the problem of ethernet, but the problem of no hardware decoder in imx93.

I have fixed the problem,  it need to add config to chromium to build h264 software decoder.

 

Best Regards

View solution in original post

0 Kudos
Reply
4 Replies
1,293 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Try the latest BSP, chromium has some bugs in the version you are playing.

Regards

0 Kudos
Reply
1,234 Views
jiangyaqiang
Contributor V

Hi Bio_TICFSL:

 

I have upgraded  to LF.6.6.36, but the issue still remain. 

Any suggestion ? 

0 Kudos
Reply
1,214 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Please send us the log file, is this your custom board or is EVK? I have the MX93EVK and everything works well on ethernet.

 

Regards

0 Kudos
Reply
1,211 Views
jiangyaqiang
Contributor V

HI Bio_TICFS:

 

Thanks .

I't's not the problem of ethernet, but the problem of no hardware decoder in imx93.

I have fixed the problem,  it need to add config to chromium to build h264 software decoder.

 

Best Regards

0 Kudos
Reply