chromium could not play video on network on imx93evk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

chromium could not play video on network on imx93evk

ソリューションへジャンプ
1,421件の閲覧回数
jiangyaqiang
Contributor V

Hi experts:

 

  I found that the chromium could not play video on network on platfrom imx93evk,

yocto: LF 6.1.55.  No log print out,  just show "network could not connect" on wed.

 Does any knows why ? 

 

  Thanks

 Best Regards

ラベル(3)
タグ(1)
0 件の賞賛
返信
1 解決策
1,323件の閲覧回数
jiangyaqiang
Contributor V

HI Bio_TICFS:

 

Thanks .

I't's not the problem of ethernet, but the problem of no hardware decoder in imx93.

I have fixed the problem,  it need to add config to chromium to build h264 software decoder.

 

Best Regards

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,406件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Try the latest BSP, chromium has some bugs in the version you are playing.

Regards

0 件の賞賛
返信
1,347件の閲覧回数
jiangyaqiang
Contributor V

Hi Bio_TICFSL:

 

I have upgraded  to LF.6.6.36, but the issue still remain. 

Any suggestion ? 

0 件の賞賛
返信
1,327件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Please send us the log file, is this your custom board or is EVK? I have the MX93EVK and everything works well on ethernet.

 

Regards

0 件の賞賛
返信
1,324件の閲覧回数
jiangyaqiang
Contributor V

HI Bio_TICFS:

 

Thanks .

I't's not the problem of ethernet, but the problem of no hardware decoder in imx93.

I have fixed the problem,  it need to add config to chromium to build h264 software decoder.

 

Best Regards

0 件の賞賛
返信