chip select line mimxrt1170

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

chip select line mimxrt1170

466 Views
sandeep_c
Contributor I

iam new software engineer and developing the driver for ksz8851snli iam getting little confusion with clock diagram of ksz8851snli which is spi to ethernet 

data sheet link of ksz8851snli page no:22

https://ww1.microchip.com/downloads/en/DeviceDoc/KSZ8851SNL-Single-Port-Ethernet-Controller-with-SPI...

txq_fifo_writing_clock_diagram.png

my requirement is to send the txfifo register address first then then i need write data to the txq fifo for this iam getting two things on mind

1) first i have to make all data to be in an single array like

tx  register address + data 

for example if i have => register address has 0x80 and data as 0x1234

int arr[10];

arr[0]= 0x80;

arr[1]=0x1234;

lpspi_transfer_t fifo_write;
fifo_write.txData=arr;
fifo_write.rxData=NULL;
fifo_write.dataSize=10;
fifo_write.configFlags=kLPSPI_MasterPcs1 | kLPSPI_MasterPcsContinuous | kLPSPI_SlaveByteSwap;
LPSPI_MasterTransferBlocking(LPSPI4,&fifo_write);

                                                                       OR

 

2)

for example if i have => register address has 0x80 and data as 0x1234

int arr[10];

arr[0]= 0x80;

lpspi_transfer_t fifo_write;
fifo_write.txData=arr;
fifo_write.rxData=NULL;
fifo_write.dataSize=10;
fifo_write.configFlags=kLPSPI_MasterPcs1 | kLPSPI_MasterPcsContinuous | kLPSPI_SlaveByteSwap;
LPSPI_MasterTransferBlocking(LPSPI4,&fifo_write);

arr[0]=0x1234;

lpspi_transfer_t fifo_write;
fifo_write.txData=arr;
fifo_write.rxData=NULL;
fifo_write.dataSize=10;
fifo_write.configFlags=kLPSPI_MasterPcs1 | kLPSPI_MasterPcsContinuous | kLPSPI_SlaveByteSwap;
LPSPI_MasterTransferBlocking(LPSPI4,&fifo_write);

NOTE: In this api chip select line be low when data starts transmitting after data transmitted chip select line will be high

WRITTEN_WAVEFORM.png 

as per the txq fifo write clock diagram can write both the ways i.e 1 and 2 or else i have to write only 1st one or else please suggent is there any way of choosing seperate chip select line low and high when ever i required it means sending all the data i need to make high

its required urgent reply 

Thank you and regards

Sandeep C

 

0 Kudos
Reply
0 Replies