changes to be made in u-boot for changing from DDR3 to LPDDR2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

changes to be made in u-boot for changing from DDR3 to LPDDR2

1,145件の閲覧回数
srinivasaporam
Contributor II

Hi,

We have  got a customized board which is designed based on Freescale's IMX6Q/IMX6DL processor board. This customized board is using LPDDR2  where as reference board is having DDR3 memory. And also reference board is designed with IMX6Q/IMX6DL where as customized board is based on IMX6D.

Now, what are the changes that we need to do in U-boot. Which are all the files those need to be modified.

ラベル(4)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,006件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Srinivasa

changes are *.cfg file with ddr configuration, location

../uboot/board/freescale/mx6sabresd and ..include/configs/*.h

board file.

Best regards

igor

0 件の賞賛
返信

1,006件の閲覧回数
srinivasaporam
Contributor II

Hi,

But my board is based on reference designs of wandboard.

0 件の賞賛
返信