change the i.MX8QM ATF UART

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

change the i.MX8QM ATF UART

2,279 Views
winters_chen
Contributor I

您好!我想要将 i.MX8QM 中的 ATF 的串口由 UART0 改为 UART4 ,我将 imx8qm_bl31_setup.c 文件中的串口基地址,串口和引脚等参数进行了修改,但是 UART4 并没有 log 输出。我是否还需要在其他地方作修改呢?能不能给我提供帮助,谢谢!

0 Kudos
Reply
2 Replies

2,222 Views
igorpadykov
NXP Employee
NXP Employee

Hi Winters

also one can look at uart settings in scfw ..platform/board/mx8qm_mek/board.c 

and sect.3.4 Compiling the Code  System Controller Firmware Porting Guide,  sc_fw_port.pdf

SCFW Porting Kit

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,222 Views
winters_chen
Contributor I

hello , it does not  help for me . I want to change the uart in atf ,not in scfw . The file you sent to me is not abot the atf . Could you give me some help ?

0 Kudos
Reply