Hello Experts,
I'm working with i.MX6 board which uses omnivision camera sensor, by default camera driver supports 1280x720 resolution @ 30fps, so i want the camera driver to support VGA,QVGA @ 15fps as well as 30 fps. so what i'm asking when changing resolution which registers affect so that i can configure only those registers. i tried contacting omnivision support team but no help so far. If any one has idea how to do that please advice me.
regards
Ganesh
you can use unit test to test the camera, then you can set format, resolution and frame rate.
Hi Guanqiong xie,
I don't have any unit test to test. do you know where i can get, please post that link.
regards,
Ganesh
do you use linux? if yes, you can use freescale bsp which includes unit test.
yes i'm using linux. i have driver source code but not bsp support at this point of time. i'm new to this.
you can download them from freescale official website as below: