Hello Everyone,
I am trying to build uboot for my custom board following the document i.MX Porting Guide, Rev. L4.14.98-2.0.0_ga, 04/2019. I am doing it through chapter 3.1.2 How to build and load U-Boot in Yocto Project.
In that 4th step mention - Copy an existing machine file associated with the SoC on custom board to the
custom layer.
cp sources/meta-freescale/conf/machine/<machine-name>.conf <new layer>/conf/machine/
<custom_name>.conf
I am looking for imx6ul evaluation kit conf. which is I supposed to be imxulevk.conf or imx6ul-14x14-evk.conf. I dont find any of these files in my ources/meta-freescale/conf/machine/.
I have build the project using commands mentioned in i.MX Yocto Project User's Guide, Rev. L4.9.88_2.0.0-ga.
mkdir imx-yocto-bsp
$ cd imx-yocto-bsp
$ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-rocko -
m imx-4.9.88-2.0.0_ga.xml
$ repo sync
where can I find the file and why is it not there?
Can someone also tell me does this linux version of rocko support imxul evaluation kit or not?
Thanks & Regards,
Asma
Solved! Go to Solution.
Hi, Asma Alekar
Yes, Yocto version L4.9.88_2.0.0-ga supports i.MX 6UltraLite EVK platform. One can check the Section 1.3 of this link.
You can find the Machine Configuration file imx6ulevk.conf at "sources/meta-fsl-bsp-release/imx/meta-bsp/conf/machine/" path.
Regards,
Radhika.
Hi, Asma Alekar
Yes, Yocto version L4.9.88_2.0.0-ga supports i.MX 6UltraLite EVK platform. One can check the Section 1.3 of this link.
You can find the Machine Configuration file imx6ulevk.conf at "sources/meta-fsl-bsp-release/imx/meta-bsp/conf/machine/" path.
Regards,
Radhika.
Thank you Radhika.
Yes it's present at that location.
Thanks for the updates. we can close this thread.