cannot download the source from repo 4.9.11.1.0.0 imx6DL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

cannot download the source from repo 4.9.11.1.0.0 imx6DL

1,307 次查看
shankovai
Contributor III

Hello support team,

i have followed the instruction given in the i.MX Yocto Project User's Guide, Rev. L4.9.11_1.0.0-ga+mx8-alpha, 09/2017

ubuntu 16.04

Packages

1.sudo apt-get install gawk wget git-core diffstat unzip texinfo gcc-multilib \
build-essential chrpath socat libsdl1.2-dev

mkdir ~/bin (this step may not be needed if the bin folder already exists)
$ curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ~/bin/repo
$ chmod a+x ~/bin/repo
2. Add the following line to the .bashrc file to ensure that the ~/bin folder is in your PATH variable.
export PATH=~/bin:$PATH

$ git config --global user.name "Your Name"
$ git config --global user.email "Your Email"
$ git config --list

mkdir fsl-release-bsp
$ cd fsl-release-bsp
$ repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-morty -m
imx-4.9.11-1.0.0_ga.xml

 

Below is the message got while downloading the source

- snippet -

repo init -u https://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp -b imx-morty -m imx-4.9.11-1.0.0_ga.xml
Traceback (most recent call last):
File "/home/shan/yocto/fsl-release-bsp/.repo/repo/main.py", line 42, in <module>
from git_config import RepoConfig
File "/home/shan/yocto/fsl-release-bsp/.repo/repo/git_config.py", line 774
self._Set(f'superproject.{key}', value)
^
SyntaxError: invalid syntax

- snippet end 

 

after installing repo and given sudo below error message

sudo repo init -u https://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp -b imx-morty
File "/home/hope/shankar/yocto/fsl-release-bsp/.repo/repo/main.py", line 79
file=sys.stderr)
^
SyntaxError: invalid syntax

 

i have tried below link also not working

http://git.freescale.com/git/cgit.cgi/imx/fsl-arm-yocto-bsp.git/tree/README?h=imx-morty

can you please provide your instruction to solve this issue

Thanks

 

0 项奖励
回复
1 回复

1,290 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi @shankovai 

The error caused by using wrong version of python. You need to change proper python for the current repo and Linux Distro. 

You can check the current version of your Host Distro for the python. which should be python3 for repo to work correctly.

 

Best regards

Harvey

0 项奖励
回复