cannot download TP2855 patch from i.MX Processors Knowledge Base

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

cannot download TP2855 patch from i.MX Processors Knowledge Base

1,694 次查看
jjiimmyy
Contributor II

Hi

I have trouble downloading a specific patch, number 6

    TP2855 + TP3812 + IMX307, patch

from

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-mx8x-ADAS-support/ta-p/1123412

1 to 5, 7,8 are OK

Please help

 

 

0 项奖励
回复
3 回复数

1,650 次查看
zoey_li
NXP Employee
NXP Employee

Hi @jjiimmyy ,

Please check the attachment.

Regards,

Zoey

1,308 次查看
sunannan
Contributor II

hi

IMX8MP可以使用tp2855吗?我看其它帖子说8MP不支持虚拟通道分离视频输入的能力,还请您确认一下,谢谢。

0 项奖励
回复

1,303 次查看
zoey_li
NXP Employee
NXP Employee

Hi @sunannan ,

Yes, 8MP does not support camera input with multi virtual channels. If connecting multi cameras to TP2855, then it can't be supported on 8MP.

Regards,

Zoey