hello experts,
I have an imx53 smd and downloaded the lucid_1108.tar.gz from freescale website.
Then use the MFG tool to flash the uboot,uImage and,lucid_1108.tar.gz into the eMMC of imx53 smd.
As I know ,lucid_1108.tar.gz is the demo image to run ubuntu on imx53 smd.
Aafter I power on my imx53 smd, the kernel and rootfs can run successfully .
From the uart console, I can login the ubuntu with the account:lucid and passwd :lucid.
But the in LCD of mx53 smd ,I can't see the ubuntu desktop. It only shows as below:
and it seems the touch screen of mx53 smd can't work in lucid_1108.tar.gz.
There is no response no matter I click anywhere on the LCD.
How can I see the ubuntu desktop?
BTW: how can I know which touch screen driver (eGalax or P1003) is in my mx53 smd ?
Hi Collin,
You can refer to the link MFGTool profile to update ubuntu image on iMX53 SMD board -blog archive to modify the ucl.xml file and download the images with ubuntu lucid_1108.tar.gz again. And the boot the board up again.
After you try, please let me know, if it work or not.
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hi Dan,
I have used the ucl.xml (in MFGTool profile to update ubuntu image on iMX53 SMD board -blog archiveMFGTool profile to update ubuntu image on iMX53 SMD board -blog archive) to download lucid_1108.tar.gz again.
But it has the same problem.
I can see log from the uart :
Last login: Thu Jan 1 08:48:55 CST 1970 on ttymxc0
Linux lucid-desktop 2.6.35.3-998-ga1cd8a7 #32 PREEMPT Wed Mar 23 10:45:18 CST 2016 armv7l GNU/Linux
Ubuntu 10.04 LTS
Welcome to Ubuntu!
* Documentation: https://help.ubuntu.com/
300 packages can be updated.
94 updates are security updates.
it means the ubuntu has already run.But it does still show the picture as above.
I search the problem in google.Some people said that the /tmp folder doesn't have permission.
I input : ls ,it shows: