can we upgrade to iMX6 quad plus from iMX6 quad without modifying the existing imx6 quad PCB?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

can we upgrade to iMX6 quad plus from iMX6 quad without modifying the existing imx6 quad PCB?

894 Views
tamilarasane
Contributor III

Hi 

iMX6 quad and iMX6 quad Plus are seems to be pin to pin compatible. I already designed a custom PCB for iMX6 Quad processor. Can I mount the iMx6 quad Plus processor in the already existing PCB ? or do I need to redesign the PCB? 

Is there any application note available to explain the hardware changes required for upgrade?

Thanks,

Tamilarasan

Labels (3)
0 Kudos
Reply
1 Reply

663 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Tamilarasan E,

There is an Engineering Bulletin covering the differences between the i.MX6D/Q and the i.MX6DP/QP (link below).

http://www.nxp.com/assets/documents/data/en/engineering-bulletins/EB810.pdf

In general the layout remains the same but the power requirements vary a little so you would need to make sure that your power supplies will provide enough power.

I hope this helps!

Regards,

0 Kudos
Reply