can the gpio pull up state keep in mem sleep mode ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

can the gpio pull up state keep in mem sleep mode ?

跳至解决方案
1,800 次查看
yan2anfei
Contributor III

hi ,

I have a imx6slevk board ,use yocto L4.1.15_2.1.0-ga.

I set a gpio to pullup state.

In  standby mode ,the pullup can keep. mem mode the pullup can't keep.

Is there any way to achieve mem mode keep the gpio pullup state?

标签 (1)
0 项奖励
回复
1 解答
1,621 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

  Mem (suspend to RAM) mode maps to DORMANT mode, meaning main i.MX6

power is off. Therefore internal i.MX6 pull up settings cannot be keep.

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

在原帖中查看解决方案

1 回复
1,622 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

  Mem (suspend to RAM) mode maps to DORMANT mode, meaning main i.MX6

power is off. Therefore internal i.MX6 pull up settings cannot be keep.

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!