can the gpio pull up state keep in mem sleep mode ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

can the gpio pull up state keep in mem sleep mode ?

Jump to solution
1,801 Views
yan2anfei
Contributor III

hi ,

I have a imx6slevk board ,use yocto L4.1.15_2.1.0-ga.

I set a gpio to pullup state.

In  standby mode ,the pullup can keep. mem mode the pullup can't keep.

Is there any way to achieve mem mode keep the gpio pullup state?

Labels (1)
0 Kudos
Reply
1 Solution
1,622 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  Mem (suspend to RAM) mode maps to DORMANT mode, meaning main i.MX6

power is off. Therefore internal i.MX6 pull up settings cannot be keep.

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

View solution in original post

1 Reply
1,623 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  Mem (suspend to RAM) mode maps to DORMANT mode, meaning main i.MX6

power is off. Therefore internal i.MX6 pull up settings cannot be keep.

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!