can't get kernel image error in imx25 pdk

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

can't get kernel image error in imx25 pdk

跳至解决方案
2,491 次查看
arumugamramasam
Contributor II

Hi,

I am using iMX25 PDK with 3 stack configuration. I have reproduced the CPU boards and using with the personality board supplied by freescale. While booting from SD card, the original CPU is booting and one of my newly produced CPUs is also booting. But without changing the SD Card, if I change the CPU, it is not booting up. Saying that can't load kernel image. The log files of good and bad booting are attached. Need help to find the reason why is it malfunctioning between CPU to CPU.

 

Thanks,

Arumugam R

Original Attachment has been moved to: Kernel-Loaded.txt.zip

Original Attachment has been moved to: Can't-get-kernel-image.txt.zip

标签 (1)
0 项奖励
回复
1 解答
1,997 次查看
jimmychan
NXP TechSupport
NXP TechSupport

Your understand is correct.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,997 次查看
jimmychan
NXP TechSupport
NXP TechSupport

Do you mean you made two identical CPU boards? Then one is good, it can boot up without any problem. The other one cannot boot up, right? According to the log, the bad one the kernel can be loaded to DDR, but it cannot be executed.

Please try to decrease the DDR freq.. Please check the DDR (hardware) soldering on the board.

0 项奖励
回复
1,997 次查看
arumugamramasam
Contributor II

Thanks for the response. But the same board boots from Nand. If in case there is any problem with DDR then it should not have booted from Nand either right? Please let me know whether my understanding is correct or not.

Thanks,

Arumugam R

0 项奖励
回复
1,998 次查看
jimmychan
NXP TechSupport
NXP TechSupport

Your understand is correct.

0 项奖励
回复