can't find file to patch at input line 4 for L5.4.70-2.3.0 BSP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

can't find file to patch at input line 4 for L5.4.70-2.3.0 BSP

1,847 次查看
ray_deng1
Contributor III

Dears,

 

When bitbake imx-image-full for L5.4.70-2.3.0 BSP, it reports 'can't find file to patch' error. I searched all project files, no such file to patch. Log attached, and onnxruntime_1.1.2.bb already modified gitsm to git due to git error.

Can you help to advice?

BRs,

Ray

标签 (1)
0 项奖励
回复
6 回复数

1,836 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

You can delete the imx-yocto-bsp and recompile it.

0 项奖励
回复

1,832 次查看
ray_deng1
Contributor III

Thanks for respnse.

Do you mean delete build-xwayland directory and recompile?

 

BRs,

Ray

0 项奖励
回复

1,824 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Yes

0 项奖励
回复

1,790 次查看
ray_deng1
Contributor III

I've tried, still cannot compile success, even I update to L5.4.70-2.3.1 version.

Do you have any advice?

 

BRs,

Ray

0 项奖励
回复

1,786 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

I have rebuilt  L5.4.70-2.3.0 BSP in different devices(Ubuntu18/20) these days...Never meet this issue...You can try to update your system packages.This should be your host pc issue

 

BR

Zhiming

0 项奖励
回复

1,779 次查看
ray_deng1
Contributor III

Hi Zhiming,

      

       Thanks for great support,

       I fellow your advice, cleaned the build-xwayland directory and modified from virtual machine to local PC, it still report the same error.

       I only modified the onneruntime-xx.bb file from “gitsm and https to git and git, can you help to advice?

       Thanks,

0 项奖励
回复