? can't find BSP for i.MX6U : MCIMX6U7CVM08AC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

? can't find BSP for i.MX6U : MCIMX6U7CVM08AC

452 Views
desireed
Contributor I


We are using ARM     i.MX6U    MCIMX6U7CVM08AC

What family does this chip fall under and which BSP do I need?

Can you post a link to this BSP for me please?
[ro.build.description]: [sabresd_6dq-user 4.3 1.1.0-rc4 20131206 dev-keys]

[ro.build.display.id]: [1.1.0-rc4]

[ro.build.fingerprint]: [Freescale/sabresd_6dq/sabresd_6dq:4.3/1.1.0-rc4/20131206:user/dev-keys]

[ro.build.host]: [madspeed]

[ro.build.id]: [1.1.0-rc4]

[ro.build.product]: [sabresd_6dq]

[ro.build.tags]: [dev-keys]

[ro.build.type]: [user]

[ro.build.user]: [b18293]

[ro.build.version.codename]: [REL]

[ro.build.version.incremental]: [20131206]

[ro.build.version.release]: [4.3]

[ro.build.version.sdk]: [18]

0 Kudos
Reply
1 Reply

358 Views
SergioSolis
NXP Employee
NXP Employee

Hello Desiree,

It is a dual processor, so you should use the i.mx6DQ

List of BSPs is here:

SABRE for Smart Devices Reference Design|Freescale

Under "run-time software"


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply