can not load the firmware from the /lib/firmware

cancel
Showing results for 
Search instead for 
Did you mean: 

can not load the firmware from the /lib/firmware

658 Views
tomgao
Contributor III

fec 2188000.ethernet eth0: registered PHC device 0
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-pci: EHCI PCI platform driver
ehci-mxc: Freescale On-Chip EHCI Host driver
xhci_hcd 0000:01:00.0: xHCI Host Controller
xhci_hcd 0000:01:00.0: new USB bus registered, assigned bus number 1
[XHCI FW Downloder] XHCI_FWDownLoadCheck

[XHCI FW Downloder] VenderID=1912, DeviceID=0014, Revision=0003
[XHCI FW Downloder] Device is 720201/202
[XHCI FW Downloder] --Revision 3
pci_bus 0000:01: firmware, attempted to load /lib/firmware/updates/3.14.28-1.0.0_ga+g91cf351/renesas/K2026090.mem, but failed with error 1
pci_bus 0000:01: firmware, attempted to load /lib/firmware/updates/renesas/K2026090.mem, but failed with error 1
pci_bus 0000:01: firmware, attempted to load /lib/firmware/3.14.28-1.0.0_ga+g91cf351/renesas/K2026090.mem, but failed with error 1
pci_bus 0000:01: firmware, attempted to load /lib/firmware/renesas/K2026090.mem, but failed with error 1
pci_bus 0000:01: Direct firmware load failed with error -2

Labels (1)
0 Kudos
2 Replies

353 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi tom

firmware may fail to load due to kernel version incompatibility,

in general one can try to debug it using AN4553 Using Open Source Debugging

Tools for Linux on i.MX Processors
http://www.nxp.com/assets/documents/data/en/application-notes/AN4553.pdf

Also every device may require different firmware version, one can try to obtain updated

firmware for that particular device from renesas.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

353 Views
tomgao
Contributor III

I have check the directory  /lib/firmware/renesas/K2026090.mem is right !

0 Kudos