I have a legacy main board that I am plugging in a custom imx6sl board. I need a single ecspi device that can select 16 different devices on the bus. My main board has a 4 bit decoder that generates a single chip select for the 16 devices.
1. is it possible to drive a 4-bit binary count out of the ecspi chips selects?
2. Can I overload a low level device driver to handle 16 spi device calls to one of the spi devices using the 4 chip selects?
3. I am currently able to run the chip select with a modified Linux kernel driver, but get stuck on address over 3 due to a issue with a "wait_for_completion in the spi_imx_transfer function. Is it possible to make this work?
Found the final solution, which involved masking the chip select so the higher numbers would not affect bits in other parts of the registers.
There may be better way to implement this this seem to work.
From the spi_imx.c file:
**************************************************
#define SPI_IMX2_3_CTRL_CS(cs) | ((cs&0x3) << 18) // RMC --- prevent cs > 3 from ovr wrt burst len |
#define SPI_IMX2_3_CTRL_BL_OFFSET 20
#define SPI_IMX2_3_CONFIG 0x0c
#define SPI_IMX2_3_CONFIG_SCLKPHA(cs) (1 << ((cs&0x3) + 0))
#define SPI_IMX2_3_CONFIG_SCLKPOL(cs) (1 << ((cs&0x3) + 4))
#define SPI_IMX2_3_CONFIG_SBBCTRL(cs) (1 << ((cs&0x3) + 8))
#define SPI_IMX2_3_CONFIG_SSBPOL(cs) (1 << ((cs&0x3) + 12))
Thanks for your reply. I have set up 4 chip selects and have coded the direction and data calls for driver and it appears to work for decodes of 0, 1, 2 and 3 but when I try to use 4 or greater it only works with single byte transfers.
Chip selects for 0, 1,2 and 3 will send many bytes but 4 or greater stops after the first byte and locks up the device. I have added printk statements in to the modified drvier. The system stops at the "wait_for_completion(&spi_imx->xfer_done)" line of the spi_imx.c driver.
I am continuing to debugg but wondering if there is a register configuration missing when using the driver this way?
Any suggestion.
Seem to currently have an issue with the spi configuration register, it look like cs values greater than 3 shift in to the burst control portion of the register.
going to see if I comment out the CONFIG_SBBCTRL line fixes my issue and does not break the NOR spi.
/*
* Copyright (C) 2004-2007, 2012 Freescale Semiconductor, Inc. All Rights Reserved.
* Copyright (C) 2008 Juergen Beisert
*
* This program is free software; you can redistribute it and/or
* modify it under the terms of the GNU General Public License
* as published by the Free Software Foundation; either version 2
* of the License, or (at your option) any later version.
* This program is distributed in the hope that it will be useful,
* but WITHOUT ANY WARRANTY; without even the implied warranty of
* MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
* GNU General Public License for more details.
*
* You should have received a copy of the GNU General Public License
* along with this program; if not, write to the
* Free Software Foundation
* 51 Franklin Street, Fifth Floor
* Boston, MA 02110-1301, USA.
*/
#include <linux/clk.h>
#include <linux/completion.h>
#include <linux/delay.h>
#include <linux/err.h>
#include <linux/gpio.h>
#include <linux/init.h>
#include <linux/interrupt.h>
#include <linux/io.h>
#include <linux/irq.h>
#include <linux/kernel.h>
#include <linux/module.h>
#include <linux/platform_device.h>
#include <linux/slab.h>
#include <linux/spi/spi.h>
#include <linux/spi/spi_bitbang.h>
#include <linux/types.h>
#include <mach/spi.h>
#define DRIVER_NAME "spi_imx"
#define MXC_CSPIRXDATA 0x00
#define MXC_CSPITXDATA 0x04
#define MXC_CSPICTRL 0x08
#define MXC_CSPIINT 0x0c
#define MXC_RESET 0x1c
#define MX3_CSPISTAT 0x14
#define MX3_CSPISTAT_RR (1 << 3)
/* generic defines to abstract from the different register layouts */
#define MXC_INT_RR (1 << 0) /* Receive data ready interrupt */
#define MXC_INT_TE (1 << 1) /* Transmit FIFO empty interrupt */
struct spi_imx_config {
unsigned int speed_hz;
unsigned int bpw;
unsigned int mode;
u8 cs;
};
enum spi_imx_devtype {
SPI_IMX_VER_IMX1,
SPI_IMX_VER_0_0,
SPI_IMX_VER_0_4,
SPI_IMX_VER_0_5,
SPI_IMX_VER_0_7,
SPI_IMX_VER_2_3,
};
struct spi_imx_data;
struct spi_imx_devtype_data {
void (*intctrl)(struct spi_imx_data *, int);
int (*config)(struct spi_imx_data *, struct spi_imx_config *);
void (*trigger)(struct spi_imx_data *);
int (*rx_available)(struct spi_imx_data *);
void (*reset)(struct spi_imx_data *);
unsigned int fifosize;
};
struct spi_imx_data {
struct spi_bitbang bitbang;
struct completion xfer_done;
void *base;
int irq;
struct clk *clk;
unsigned long spi_clk;
int *chipselect;
unsigned int count;
void (*tx)(struct spi_imx_data *);
void (*rx)(struct spi_imx_data *);
void *rx_buf;
const void *tx_buf;
unsigned int txfifo; /* number of words pushed in tx FIFO */
struct spi_imx_devtype_data devtype_data;
};
#define MXC_SPI_BUF_RX(type) \
static void spi_imx_buf_rx_##type(struct spi_imx_data *spi_imx) \
{ \
unsigned int val = readl(spi_imx->base + MXC_CSPIRXDATA); \
\
if (spi_imx->rx_buf) { \
*(type *)spi_imx->rx_buf = val; \
spi_imx->rx_buf += sizeof(type); \
} \
}
#define MXC_SPI_BUF_TX(type) \
static void spi_imx_buf_tx_##type(struct spi_imx_data *spi_imx) \
{ \
type val = 0; \
\
if (spi_imx->tx_buf) { \
val = *(type *)spi_imx->tx_buf; \
spi_imx->tx_buf += sizeof(type); \
} \
\
spi_imx->count -= sizeof(type); \
\
writel(val, spi_imx->base + MXC_CSPITXDATA); \
}
MXC_SPI_BUF_RX(u8)
MXC_SPI_BUF_TX(u8)
MXC_SPI_BUF_RX(u16)
MXC_SPI_BUF_TX(u16)
MXC_SPI_BUF_RX(u32)
MXC_SPI_BUF_TX(u32)
/* First entry is reserved, second entry is valid only if SDHC_SPIEN is set
* (which is currently not the case in this driver)
*/
static int mxc_clkdivs[] = {0, 3, 4, 6, 8, 12, 16, 24, 32, 48, 64, 96, 128, 192,
256, 384, 512, 768, 1024};
/* MX21, MX27 */
static unsigned int spi_imx_clkdiv_1(unsigned int fin,
unsigned int fspi)
{
int i, max;
printk("RMC ---- func:spi_imx_clkdiv --\n");
if (cpu_is_mx21())
max = 18;
else
max = 16;
for (i = 2; i < max; i++)
if (fspi * mxc_clkdivs[i] >= fin)
return i;
return max;
}
/* MX1, MX31, MX35, MX51 CSPI */
static unsigned int spi_imx_clkdiv_2(unsigned int fin,
unsigned int fspi)
{
int i, div = 4;
printk("RMC ---- func:spi_imx_clkdiv_2 --\n");
for (i = 0; i < 7; i++) {
if (fspi * div >= fin)
return i;
div <<= 1;
}
return 7;
}
#define SPI_IMX2_3_CTRL 0x08
#define SPI_IMX2_3_CTRL_ENABLE (1 << 0)
#define SPI_IMX2_3_CTRL_XCH (1 << 2)
#define SPI_IMX2_3_CTRL_MODE_MASK (0xf << 4)
#define SPI_IMX2_3_CTRL_POSTDIV_OFFSET 8
#define SPI_IMX2_3_CTRL_PREDIV_OFFSET 12
#define SPI_IMX2_3_CTRL_CS(cs) ((cs) << 18)
#define SPI_IMX2_3_CTRL_BL_OFFSET 20
#define SPI_IMX2_3_CONFIG 0x0c
#define SPI_IMX2_3_CONFIG_SCLKPHA(cs) (1 << ((cs) + 0))
#define SPI_IMX2_3_CONFIG_SCLKPOL(cs) (1 << ((cs) + 4))
#define SPI_IMX2_3_CONFIG_SBBCTRL(cs) (1 << ((cs) + 8))
#define SPI_IMX2_3_CONFIG_SSBPOL(cs) (1 << ((cs) + 12))
#define SPI_IMX2_3_INT 0x10
#define SPI_IMX2_3_INT_TEEN (1 << 0)
#define SPI_IMX2_3_INT_RREN (1 << 3)
#define SPI_IMX2_3_STAT 0x18
#define SPI_IMX2_3_STAT_RR (1 << 3)
/* MX51 eCSPI */
static unsigned int spi_imx2_3_clkdiv(unsigned int fin, unsigned int fspi)
{
/*
* there are two 4-bit dividers, the pre-divider divides by
* $pre, the post-divider by 2^$post
*/
unsigned int pre, post;
printk("RMC ---- func:spi_imx2_3_clkdiv --\n");
if (unlikely(fspi > fin))
return 0;
post = fls(fin) - fls(fspi);
if (fin > fspi << post)
post++;
/* now we have: (fin <= fspi << post) with post being minimal */
post = max(4U, post) - 4;
if (unlikely(post > 0xf)) {
pr_err("%s: cannot set clock freq: %u (base freq: %u)\n",
__func__, fspi, fin);
return 0xff;
}
pre = DIV_ROUND_UP(fin, fspi << post) - 1;
pr_debug("%s: fin: %u, fspi: %u, post: %u, pre: %u\n",
__func__, fin, fspi, post, pre);
return (pre << SPI_IMX2_3_CTRL_PREDIV_OFFSET) |
(post << SPI_IMX2_3_CTRL_POSTDIV_OFFSET);
}
static void __maybe_unused spi_imx2_3_intctrl(struct spi_imx_data *spi_imx, int enable)
{
unsigned val = 0;
printk("RMC ---- func:spi2_3_imx_intctrl --\n");
if (enable & MXC_INT_TE)
val |= SPI_IMX2_3_INT_TEEN;
if (enable & MXC_INT_RR)
val |= SPI_IMX2_3_INT_RREN;
writel(val, spi_imx->base + SPI_IMX2_3_INT);
printk("RMC ---- func:spi2_3_imx_intctrl exit after writel --\n");
}
static void __maybe_unused spi_imx2_3_trigger(struct spi_imx_data *spi_imx)
{
u32 reg;
reg = readl(spi_imx->base + SPI_IMX2_3_CTRL);
reg |= SPI_IMX2_3_CTRL_XCH;
writel(reg, spi_imx->base + SPI_IMX2_3_CTRL);
}
static int __maybe_unused spi_imx2_3_config(struct spi_imx_data *spi_imx,
struct spi_imx_config *config)
{
u32 ctrl = SPI_IMX2_3_CTRL_ENABLE, cfg = 0;
/*
* The hardware seems to have a race condition when changing modes. The
* current assumption is that the selection of the channel arrives
* earlier in the hardware than the mode bits when they are written at
* the same time.
* So set master mode for all channels as we do not support slave mode.
*/
ctrl |= SPI_IMX2_3_CTRL_MODE_MASK;
/* set clock speed */
ctrl |= spi_imx2_3_clkdiv(spi_imx->spi_clk, config->speed_hz);
/* set chip select to use */
ctrl |= SPI_IMX2_3_CTRL_CS(config->cs);
ctrl |= (config->bpw - 1) << SPI_IMX2_3_CTRL_BL_OFFSET;
//RMC --- cfg |= SPI_IMX2_3_CONFIG_SBBCTRL(config->cs); //persistor chip sel fix all forces all other to ch0 only
if (config->mode & SPI_CPHA)
cfg |= SPI_IMX2_3_CONFIG_SCLKPHA(config->cs);
if (config->mode & SPI_CPOL)
cfg |= SPI_IMX2_3_CONFIG_SCLKPOL(config->cs);
if (config->mode & SPI_CS_HIGH)
cfg |= SPI_IMX2_3_CONFIG_SSBPOL(config->cs);
printk("RMC ---- func:__maybe_unused spi_imx2_3_config CTRL_REG=> 0x%x --\n", ctrl);
writel(ctrl, spi_imx->base + SPI_IMX2_3_CTRL);
writel(cfg, spi_imx->base + SPI_IMX2_3_CONFIG);
return 0;
}
static int __maybe_unused spi_imx2_3_rx_available(struct spi_imx_data *spi_imx)
{
return readl(spi_imx->base + SPI_IMX2_3_STAT) & SPI_IMX2_3_STAT_RR;
}
static void __maybe_unused spi_imx2_3_reset(struct spi_imx_data *spi_imx)
{
/* drain receive buffer */
while (spi_imx2_3_rx_available(spi_imx))
readl(spi_imx->base + MXC_CSPIRXDATA);
}
#define MX31_INTREG_TEEN (1 << 0)
#define MX31_INTREG_RREN (1 << 3)
#define MX31_CSPICTRL_ENABLE (1 << 0)
#define MX31_CSPICTRL_MASTER (1 << 1)
#define MX31_CSPICTRL_XCH (1 << 2)
#define MX31_CSPICTRL_POL (1 << 4)
#define MX31_CSPICTRL_PHA (1 << 5)
#define MX31_CSPICTRL_SSCTL (1 << 6)
#define MX31_CSPICTRL_SSPOL (1 << 7)
#define MX31_CSPICTRL_BC_SHIFT 8
#define MX35_CSPICTRL_BL_SHIFT 20
#define MX31_CSPICTRL_CS_SHIFT 24
#define MX35_CSPICTRL_CS_SHIFT 12
#define MX31_CSPICTRL_DR_SHIFT 16
#define MX31_CSPISTATUS 0x14
#define MX31_STATUS_RR (1 << 3)
/* These functions also work for the i.MX35, but be aware that
* the i.MX35 has a slightly different register layout for bits
* we do not use here.
*/
static void __maybe_unused mx31_intctrl(struct spi_imx_data *spi_imx, int enable)
{
unsigned int val = 0;
if (enable & MXC_INT_TE)
val |= MX31_INTREG_TEEN;
if (enable & MXC_INT_RR)
val |= MX31_INTREG_RREN;
writel(val, spi_imx->base + MXC_CSPIINT);
}
static void __maybe_unused mx31_trigger(struct spi_imx_data *spi_imx)
{
unsigned int reg;
reg = readl(spi_imx->base + MXC_CSPICTRL);
reg |= MX31_CSPICTRL_XCH;
writel(reg, spi_imx->base + MXC_CSPICTRL);
}
static int __maybe_unused spi_imx0_4_config(struct spi_imx_data *spi_imx,
struct spi_imx_config *config)
{
unsigned int reg = MX31_CSPICTRL_ENABLE | MX31_CSPICTRL_MASTER;
int cs = spi_imx->chipselect[config->cs];
reg |= spi_imx_clkdiv_2(spi_imx->spi_clk, config->speed_hz) <<
MX31_CSPICTRL_DR_SHIFT;
reg |= (config->bpw - 1) << MX31_CSPICTRL_BC_SHIFT;
if (config->mode & SPI_CPHA)
reg |= MX31_CSPICTRL_PHA;
if (config->mode & SPI_CPOL)
reg |= MX31_CSPICTRL_POL;
if (config->mode & SPI_CS_HIGH)
reg |= MX31_CSPICTRL_SSPOL;
if (cs < 0)
reg |= (cs + 32) << MX31_CSPICTRL_CS_SHIFT;
writel(reg, spi_imx->base + MXC_CSPICTRL);
return 0;
}
static int __maybe_unused spi_imx0_7_config(struct spi_imx_data *spi_imx,
struct spi_imx_config *config)
{
unsigned int reg = MX31_CSPICTRL_ENABLE | MX31_CSPICTRL_MASTER;
int cs = spi_imx->chipselect[config->cs];
reg |= spi_imx_clkdiv_2(spi_imx->spi_clk, config->speed_hz) <<
MX31_CSPICTRL_DR_SHIFT;
reg |= (config->bpw - 1) << MX35_CSPICTRL_BL_SHIFT;
reg |= MX31_CSPICTRL_SSCTL;
if (config->mode & SPI_CPHA)
reg |= MX31_CSPICTRL_PHA;
if (config->mode & SPI_CPOL)
reg |= MX31_CSPICTRL_POL;
if (config->mode & SPI_CS_HIGH)
reg |= MX31_CSPICTRL_SSPOL;
if (cs < 0)
reg |= (cs + 32) << MX35_CSPICTRL_CS_SHIFT;
writel(reg, spi_imx->base + MXC_CSPICTRL);
return 0;
}
static int __maybe_unused mx31_rx_available(struct spi_imx_data *spi_imx)
{
return readl(spi_imx->base + MX31_CSPISTATUS) & MX31_STATUS_RR;
}
static void __maybe_unused spi_imx0_4_reset(struct spi_imx_data *spi_imx)
{
/* drain receive buffer */
while (readl(spi_imx->base + MX3_CSPISTAT) & MX3_CSPISTAT_RR)
readl(spi_imx->base + MXC_CSPIRXDATA);
}
#define MX27_INTREG_RR (1 << 4)
#define MX27_INTREG_TEEN (1 << 9)
#define MX27_INTREG_RREN (1 << 13)
#define MX27_CSPICTRL_POL (1 << 5)
#define MX27_CSPICTRL_PHA (1 << 6)
#define MX27_CSPICTRL_SSPOL (1 << 8)
#define MX27_CSPICTRL_XCH (1 << 9)
#define MX27_CSPICTRL_ENABLE (1 << 10)
#define MX27_CSPICTRL_MASTER (1 << 11)
#define MX27_CSPICTRL_DR_SHIFT 14
#define MX27_CSPICTRL_CS_SHIFT 19
static void __maybe_unused mx27_intctrl(struct spi_imx_data *spi_imx, int enable)
{
unsigned int val = 0;
if (enable & MXC_INT_TE)
val |= MX27_INTREG_TEEN;
if (enable & MXC_INT_RR)
val |= MX27_INTREG_RREN;
writel(val, spi_imx->base + MXC_CSPIINT);
}
static void __maybe_unused mx27_trigger(struct spi_imx_data *spi_imx)
{
unsigned int reg;
reg = readl(spi_imx->base + MXC_CSPICTRL);
reg |= MX27_CSPICTRL_XCH;
writel(reg, spi_imx->base + MXC_CSPICTRL);
}
static int __maybe_unused mx27_config(struct spi_imx_data *spi_imx,
struct spi_imx_config *config)
{
unsigned int reg = MX27_CSPICTRL_ENABLE | MX27_CSPICTRL_MASTER;
int cs = spi_imx->chipselect[config->cs];
reg |= spi_imx_clkdiv_1(spi_imx->spi_clk, config->speed_hz) <<
MX27_CSPICTRL_DR_SHIFT;
reg |= config->bpw - 1;
if (config->mode & SPI_CPHA)
reg |= MX27_CSPICTRL_PHA;
if (config->mode & SPI_CPOL)
reg |= MX27_CSPICTRL_POL;
if (config->mode & SPI_CS_HIGH)
reg |= MX27_CSPICTRL_SSPOL;
if (cs < 0)
reg |= (cs + 32) << MX27_CSPICTRL_CS_SHIFT;
writel(reg, spi_imx->base + MXC_CSPICTRL);
return 0;
}
static int __maybe_unused mx27_rx_available(struct spi_imx_data *spi_imx)
{
return readl(spi_imx->base + MXC_CSPIINT) & MX27_INTREG_RR;
}
static void __maybe_unused spi_imx0_0_reset(struct spi_imx_data *spi_imx)
{
writel(1, spi_imx->base + MXC_RESET);
}
#define MX1_INTREG_RR (1 << 3)
#define MX1_INTREG_TEEN (1 << 8)
#define MX1_INTREG_RREN (1 << 11)
#define MX1_CSPICTRL_POL (1 << 4)
#define MX1_CSPICTRL_PHA (1 << 5)
#define MX1_CSPICTRL_XCH (1 << 8)
#define MX1_CSPICTRL_ENABLE (1 << 9)
#define MX1_CSPICTRL_MASTER (1 << 10)
#define MX1_CSPICTRL_DR_SHIFT 13
static void __maybe_unused mx1_intctrl(struct spi_imx_data *spi_imx, int enable)
{
unsigned int val = 0;
if (enable & MXC_INT_TE)
val |= MX1_INTREG_TEEN;
if (enable & MXC_INT_RR)
val |= MX1_INTREG_RREN;
writel(val, spi_imx->base + MXC_CSPIINT);
}
static void __maybe_unused mx1_trigger(struct spi_imx_data *spi_imx)
{
unsigned int reg;
reg = readl(spi_imx->base + MXC_CSPICTRL);
reg |= MX1_CSPICTRL_XCH;
writel(reg, spi_imx->base + MXC_CSPICTRL);
}
static int __maybe_unused mx1_config(struct spi_imx_data *spi_imx,
struct spi_imx_config *config)
{
unsigned int reg = MX1_CSPICTRL_ENABLE | MX1_CSPICTRL_MASTER;
reg |= spi_imx_clkdiv_2(spi_imx->spi_clk, config->speed_hz) <<
MX1_CSPICTRL_DR_SHIFT;
reg |= config->bpw - 1;
if (config->mode & SPI_CPHA)
reg |= MX1_CSPICTRL_PHA;
if (config->mode & SPI_CPOL)
reg |= MX1_CSPICTRL_POL;
writel(reg, spi_imx->base + MXC_CSPICTRL);
return 0;
}
static int __maybe_unused mx1_rx_available(struct spi_imx_data *spi_imx)
{
return readl(spi_imx->base + MXC_CSPIINT) & MX1_INTREG_RR;
}
static void __maybe_unused mx1_reset(struct spi_imx_data *spi_imx)
{
writel(1, spi_imx->base + MXC_RESET);
}
/*
* These version numbers are taken from the Freescale driver. Unfortunately it
* doesn't support i.MX1, so this entry doesn't match the scheme. :-(
*/
static struct spi_imx_devtype_data spi_imx_devtype_data[] __devinitdata = {
#ifdef CONFIG_SPI_IMX_VER_IMX1
[SPI_IMX_VER_IMX1] = {
.intctrl = mx1_intctrl,
.config = mx1_config,
.trigger = mx1_trigger,
.rx_available = mx1_rx_available,
.reset = mx1_reset,
.fifosize = 8,
},
#endif
#ifdef CONFIG_SPI_IMX_VER_0_0
[SPI_IMX_VER_0_0] = {
.intctrl = mx27_intctrl,
.config = mx27_config,
.trigger = mx27_trigger,
.rx_available = mx27_rx_available,
.reset = spi_imx0_0_reset,
.fifosize = 8,
},
#endif
#ifdef CONFIG_SPI_IMX_VER_0_4
[SPI_IMX_VER_0_4] = {
.intctrl = mx31_intctrl,
.config = spi_imx0_4_config,
.trigger = mx31_trigger,
.rx_available = mx31_rx_available,
.reset = spi_imx0_4_reset,
.fifosize = 8,
},
#endif
#ifdef CONFIG_SPI_IMX_VER_0_7
[SPI_IMX_VER_0_7] = {
.intctrl = mx31_intctrl,
.config = spi_imx0_7_config,
.trigger = mx31_trigger,
.rx_available = mx31_rx_available,
.reset = spi_imx0_4_reset,
.fifosize = 8,
},
#endif
#ifdef CONFIG_SPI_IMX_VER_2_3
[SPI_IMX_VER_2_3] = {
.intctrl = spi_imx2_3_intctrl,
.config = spi_imx2_3_config,
.trigger = spi_imx2_3_trigger,
.rx_available = spi_imx2_3_rx_available,
.reset = spi_imx2_3_reset,
.fifosize = 64,
},
#endif
};
/* wwalton@teledyne.com - 23 Sep 2013
* Action: Changed the chipselect mechanism to be hard wired for SD3_DAT0 to SD3_DAT3
* pins instead of the pin specified mx6_evk_spi_cs[] in board-mx6sl_evk.c
* Instead, mx6_evk_spi_cs[] now contains numbers 0-15, representing 16 possible
* channels, but the chipselect will use our mechanism instead of having 16
* separate chipselect pins.
* Reason: We needed to use 4 chipselect lines that are bit-encoded to match the Persistor
* chipselect mechanism
* Note: Currently, the SD3_DAT0 to SD3_DAT3 pins are used for the chipselects,
* however, you can use any other pins as long as the four pins are on the same
* port. Being on the same port allows us to change all four values simultaneously
* with one write operation. Refer to imx6sl reference manual for register
* descriptions as well as mapping of pad name to gpio port and pin.
*
*/
/*
We use the pins SD3_DAT0, SD3_DAT1, SD3_DAT2, and SD3_DAT3 for the four chip select lines.
These are all on GPIO bank 5 when configured for alternate function 5 (ALT5).
SD3_DAT0 -> GPIO5_IO19
SD3_DAT1 -> GPIO5_IO20
SD3_DAT2 -> GPIO5_IO16
SD3_DAT3 -> GPIO5_IO17
*/
#define SPI_CS_GPIO_BASEADDR 0x020ac000 // Base address for GPIO port 5
#define SPI_CS_MASK 0x001b0000 // Modify only the relevant bits on GPIO5 (19,20,16,17)
static int chan_to_bits[16] =
{
0xffffffff,
0xfff7ffff,
0xffefffff,
0xffe7ffff,
0xfffeffff,
0xfff6ffff,
0xffeeffff,
0xffe6ffff,
0xfffdffff,
0xfff5ffff,
0xffedffff,
0xffe5ffff,
0xfffcffff,
0xfff4ffff,
0xffecffff,
0xffe4ffff,
};
static void spi_imx_chipselect(struct spi_device *spi, int is_active)
{
struct spi_imx_data *spi_imx = spi_master_get_devdata(spi->master);
int gpio = spi_imx->chipselect[spi->chip_select];
int active = is_active != BITBANG_CS_INACTIVE;
int dev_is_lowactive = !(spi->mode & SPI_CS_HIGH);
void __iomem *base;
unsigned int temp;
printk("RMC ---- func:spi_imx_cs SPI_BUSS => 0x%x --\n", spi->master->bus_num);
printk("RMC ---- func:spi_imx_cs gpio => 0x%x, this the mux ch -- \n", gpio);
/* if this is the SPI bus on the persistor header (ECSPI3, or bus_num = 2), then
* we need the special mechanism for chipselect that bypasses everything and sets
* the multiplexed CS pins immediately (this needs to happen fast).
*/
if(spi->master->bus_num == 2)
{
if(gpio < 0){
return;
}
if(!active){
gpio = 0; // RMC --- defining 0 as inactive state to main board mux
}
printk("RMC ---- this is func spi_imx_chipsel spi ch=> 0x%x --\n", spi->master->num_chipselect);
base = ioremap(SPI_CS_GPIO_BASEADDR, 1024);
// write the actual GPIO value to the bank
temp = __raw_readl(base);
printk("RMC ---- func spi_imx_chipsel read GPIO data value -- %#x \n", temp);
temp |= (chan_to_bits[gpio] & SPI_CS_MASK);
temp &= (chan_to_bits[gpio] | ~SPI_CS_MASK);
__raw_writel(temp, base);
printk("RMC ---- func spi_imx_chipsel set GPIO data value -- %#x \n", temp);
wmb();
iounmap(base);
}
else
{
if (gpio < 0)
return;
gpio_set_value(gpio, dev_is_lowactive ^ active);
printk("RMC ---- func spi_imx_chipsel Master != 2, devActLow GPIO -> %#x \n", gpio);
}
}
static void spi_imx_push(struct spi_imx_data *spi_imx)
{
printk("RMC ---- func:spi_imx_push --\n");
while (spi_imx->txfifo < spi_imx->devtype_data.fifosize) {
if (!spi_imx->count)
break;
spi_imx->tx(spi_imx);
spi_imx->txfifo++;
}
spi_imx->devtype_data.trigger(spi_imx);
}
static irqreturn_t spi_imx_isr(int irq, void *dev_id)
{
printk("RMC ---- func:spi_imx_isr --\n");
struct spi_imx_data *spi_imx = dev_id;
while (spi_imx->devtype_data.rx_available(spi_imx)) {
spi_imx->rx(spi_imx);
spi_imx->txfifo--;
}
if (spi_imx->count) {
spi_imx_push(spi_imx);
return IRQ_HANDLED;
}
if (spi_imx->txfifo) {
/* No data left to push, but still waiting for rx data,
* enable receive data available interrupt.
*/
spi_imx->devtype_data.intctrl(
spi_imx, MXC_INT_RR);
return IRQ_HANDLED;
}
spi_imx->devtype_data.intctrl(spi_imx, 0);
complete(&spi_imx->xfer_done);
return IRQ_HANDLED;
}
static int spi_imx_setupxfer(struct spi_device *spi,
struct spi_transfer *t)
{
struct spi_imx_data *spi_imx = spi_master_get_devdata(spi->master);
struct spi_imx_config config;
printk("RMC ---- func:spi_imx_setupxfer --\n");
clk_enable(spi_imx->clk);
config.bpw = t ? t->bits_per_word : spi->bits_per_word;
config.speed_hz = t ? t->speed_hz : spi->max_speed_hz;
config.mode = spi->mode;
config.cs = spi->chip_select;
if (!config.speed_hz)
config.speed_hz = spi->max_speed_hz;
if (!config.bpw)
config.bpw = spi->bits_per_word;
if (!config.speed_hz)
config.speed_hz = spi->max_speed_hz;
/* Initialize the functions for transfer */
if (config.bpw <= 8) {
spi_imx->rx = spi_imx_buf_rx_u8;
spi_imx->tx = spi_imx_buf_tx_u8;
} else if (config.bpw <= 16) {
spi_imx->rx = spi_imx_buf_rx_u16;
spi_imx->tx = spi_imx_buf_tx_u16;
} else if (config.bpw <= 32) {
spi_imx->rx = spi_imx_buf_rx_u32;
spi_imx->tx = spi_imx_buf_tx_u32;
} else
BUG();
spi_imx->devtype_data.config(spi_imx, &config);
clk_disable(spi_imx->clk);
return 0;
}
static void spi_imx_print_structure(struct spi_imx_data *spi_imx){
printk("RMC ------------------- spi_imx_data STRUCTURE -------------------------");
printk("RMC ------Bitbang--------\n");
printk("RMC -----busy = %d \n", spi_imx->bitbang.busy);
printk("RMC -----use_dma = %d \n", spi_imx->bitbang.use_dma);
printk("RMC -----flags = %d \n", spi_imx->bitbang.flags);
printk("\nRMC ------Bitbang->Master --------\n");
printk("RMC -----bus_num = %d \n", spi_imx->bitbang.master->bus_num);
printk("RMC -----num_chipselect = %d \n", spi_imx->bitbang.master->num_chipselect);
printk("RMC -----dma_alignment = %d \n", spi_imx->bitbang.master->dma_alignment);
printk("RMC -----mode_bits = 0x%x \n", spi_imx->bitbang.master->mode_bits);
printk("RMC -----flags = 0x%x \n", spi_imx->bitbang.master->flags);
printk("RMC -----bus_lock_flag = 0x%x \n", spi_imx->bitbang.master->bus_lock_flag);
printk("\nRMC ------spi_imx --------\n");
printk("RMC -----spi_clk = %ld \n", spi_imx->spi_clk);
printk("RMC -----chipselect = %d \n", *(spi_imx->chipselect));
printk("RMC -----chipselect addr = %ld \n", (unsigned long)(spi_imx->chipselect));
printk("RMC -----count = %d \n", spi_imx->count);
printk("RMC -----txfifo = %d \n", spi_imx->txfifo);
printk("\nRMC ------completion --------\n");
printk("RMC -----done = %d \n", spi_imx->xfer_done.done);
printk("RMC ------------------- spi_imx_data STRUCTURE END-------------------------");
}
static int spi_imx_transfer(struct spi_device *spi,
struct spi_transfer *transfer)
{
struct spi_imx_data *spi_imx = spi_master_get_devdata(spi->master);
printk("RMC ---- func:spi_imx_transfer --\n");
clk_enable(spi_imx->clk);
spi_imx->tx_buf = transfer->tx_buf;
spi_imx->rx_buf = transfer->rx_buf;
spi_imx->count = transfer->len;
spi_imx->txfifo = 0;
init_completion(&spi_imx->xfer_done);
spi_imx_push(spi_imx);
spi_imx->devtype_data.intctrl(spi_imx, MXC_INT_TE);
printk("RMC ---- func:spi_imx_transfer start wait--\n");
spi_imx_print_structure(spi_imx); // RMC --- added printk for spi_imx struct
wait_for_completion(&spi_imx->xfer_done);
printk("RMC ---- func:spi_imx_transfer end wait--\n");
spi_imx_print_structure(spi_imx);
clk_disable(spi_imx->clk);
return transfer->len;
}
static int spi_imx_setup(struct spi_device *spi)
{
struct spi_imx_data *spi_imx = spi_master_get_devdata(spi->master);
int gpio = spi_imx->chipselect[spi->chip_select];
dev_dbg(&spi->dev, "%s: mode %d, %u bpw, %d hz\n", __func__,
spi->mode, spi->bits_per_word, spi->max_speed_hz);
if (gpio >= 0){
if(spi->master->bus_num == 2){
void __iomem *base;
unsigned int temp;
base = ioremap(SPI_CS_GPIO_BASEADDR, 1024);
//printk("RMC ---- func spi_imx_chipsel read base value -- %#x \n", *base);
// set GPIO direction to output
temp = __raw_readl(base + 0x00000004);
printk("RMC ---- func spi_imx_setup read GPIO dir value -- %#x \n", temp);
temp |= (0xffffffff & SPI_CS_MASK);
printk("RMC ---- func spi_imx_setup or GPIO dir value -- %#x \n", temp);
temp &= (0xffffffff | ~SPI_CS_MASK);
printk("RMC ---- func spi_imx_setup and GPIO dir value -- %#x \n", temp);
__raw_writel(temp, (base + 0x00000004));
printk("RMC --- func spi_imx_setup set gpio dir 0x%x \n",temp);
wmb();
iounmap(base);
}
else{
gpio_direction_output(gpio, spi->mode & SPI_CS_HIGH ? 0 : 1);
}
}
spi_imx_chipselect(spi, BITBANG_CS_INACTIVE);
return 0;
}
static void spi_imx_cleanup(struct spi_device *spi)
{
printk("RMC ---- func:spi_imx_cleanup --\n");
}
static struct platform_device_id spi_imx_devtype[] = {
{
.name = "imx1-cspi",
.driver_data = SPI_IMX_VER_IMX1,
}, {
.name = "imx21-cspi",
.driver_data = SPI_IMX_VER_0_0,
}, {
.name = "imx25-cspi",
.driver_data = SPI_IMX_VER_0_7,
}, {
.name = "imx27-cspi",
.driver_data = SPI_IMX_VER_0_0,
}, {
.name = "imx31-cspi",
.driver_data = SPI_IMX_VER_0_4,
}, {
.name = "imx35-cspi",
.driver_data = SPI_IMX_VER_0_7,
}, {
.name = "imx50-cspi",
.driver_data = SPI_IMX_VER_0_7,
}, {
.name = "imx51-cspi",
.driver_data = SPI_IMX_VER_0_7,
}, {
.name = "imx51-ecspi",
.driver_data = SPI_IMX_VER_2_3,
}, {
.name = "imx53-cspi",
.driver_data = SPI_IMX_VER_0_7,
}, {
.name = "imx53-ecspi",
.driver_data = SPI_IMX_VER_2_3,
}, {
.name = "imx6q-ecspi",
.driver_data = SPI_IMX_VER_2_3,
}, {
/* sentinel */
}
};
static int __devinit spi_imx_probe(struct platform_device *pdev)
{
struct spi_imx_master *mxc_platform_info;
struct spi_master *master;
struct spi_imx_data *spi_imx;
struct resource *res;
int i, ret;
mxc_platform_info = dev_get_platdata(&pdev->dev);
if (!mxc_platform_info) {
dev_err(&pdev->dev, "can't get the platform data\n");
return -EINVAL;
}
master = spi_alloc_master(&pdev->dev, sizeof(struct spi_imx_data));
if (!master)
return -ENOMEM;
platform_set_drvdata(pdev, master);
master->bus_num = pdev->id;
master->num_chipselect = mxc_platform_info->num_chipselect;
spi_imx = spi_master_get_devdata(master);
spi_imx->bitbang.master = spi_master_get(master);
spi_imx->chipselect = mxc_platform_info->chipselect;
for (i = 0; i < master->num_chipselect; i++) {
if (spi_imx->chipselect[i] < 0)
continue;
ret = gpio_request(spi_imx->chipselect[i], DRIVER_NAME);
if (ret) {
while (i > 0) {
i--;
if (spi_imx->chipselect[i] >= 0)
//RMC --- muxed gpio may cause issues with this function, check later.
gpio_free(spi_imx->chipselect[i]);
}
dev_err(&pdev->dev, "can't get cs gpios\n");
goto out_master_put;
}
}
spi_imx->bitbang.chipselect = spi_imx_chipselect;
spi_imx->bitbang.setup_transfer = spi_imx_setupxfer;
spi_imx->bitbang.txrx_bufs = spi_imx_transfer;
spi_imx->bitbang.master->setup = spi_imx_setup;
spi_imx->bitbang.master->cleanup = spi_imx_cleanup;
spi_imx->bitbang.master->mode_bits = SPI_CPOL | SPI_CPHA | SPI_CS_HIGH;
init_completion(&spi_imx->xfer_done);
spi_imx->devtype_data =
spi_imx_devtype_data[pdev->id_entry->driver_data];
res = platform_get_resource(pdev, IORESOURCE_MEM, 0);
if (!res) {
dev_err(&pdev->dev, "can't get platform resource\n");
ret = -ENOMEM;
goto out_gpio_free;
}
if (!request_mem_region(res->start, resource_size(res), pdev->name)) {
dev_err(&pdev->dev, "request_mem_region failed\n");
ret = -EBUSY;
goto out_gpio_free;
}
spi_imx->base = ioremap(res->start, resource_size(res));
if (!spi_imx->base) {
ret = -EINVAL;
goto out_release_mem;
}
spi_imx->irq = platform_get_irq(pdev, 0);
if (spi_imx->irq < 0) {
ret = -EINVAL;
goto out_iounmap;
}
ret = request_irq(spi_imx->irq, spi_imx_isr, 0, DRIVER_NAME, spi_imx);
if (ret) {
dev_err(&pdev->dev, "can't get irq%d: %d\n", spi_imx->irq, ret);
goto out_iounmap;
}
spi_imx->clk = clk_get(&pdev->dev, NULL);
if (IS_ERR(spi_imx->clk)) {
dev_err(&pdev->dev, "unable to get clock\n");
ret = PTR_ERR(spi_imx->clk);
goto out_free_irq;
}
clk_enable(spi_imx->clk);
spi_imx->spi_clk = clk_get_rate(spi_imx->clk);
spi_imx->devtype_data.reset(spi_imx);
spi_imx->devtype_data.intctrl(spi_imx, 0);
ret = spi_bitbang_start(&spi_imx->bitbang);
if (ret) {
dev_err(&pdev->dev, "bitbang start failed with %d\n", ret);
goto out_clk_put;
}
clk_disable(spi_imx->clk);
dev_info(&pdev->dev, "probed\n");
return ret;
out_clk_put:
clk_disable(spi_imx->clk);
clk_put(spi_imx->clk);
out_free_irq:
free_irq(spi_imx->irq, spi_imx);
out_iounmap:
iounmap(spi_imx->base);
out_release_mem:
release_mem_region(res->start, resource_size(res));
out_gpio_free:
for (i = 0; i < master->num_chipselect; i++)
if (spi_imx->chipselect[i] >= 0)
gpio_free(spi_imx->chipselect[i]);
out_master_put:
spi_master_put(master);
kfree(master);
platform_set_drvdata(pdev, NULL);
return ret;
}
static int __devexit spi_imx_remove(struct platform_device *pdev)
{
struct spi_master *master = platform_get_drvdata(pdev);
struct resource *res = platform_get_resource(pdev, IORESOURCE_MEM, 0);
struct spi_imx_data *spi_imx = spi_master_get_devdata(master);
int i;
spi_bitbang_stop(&spi_imx->bitbang);
clk_enable(spi_imx->clk);
writel(0, spi_imx->base + MXC_CSPICTRL);
clk_disable(spi_imx->clk);
clk_put(spi_imx->clk);
free_irq(spi_imx->irq, spi_imx);
iounmap(spi_imx->base);
for (i = 0; i < master->num_chipselect; i++)
if (spi_imx->chipselect[i] >= 0)
gpio_free(spi_imx->chipselect[i]);
spi_master_put(master);
release_mem_region(res->start, resource_size(res));
platform_set_drvdata(pdev, NULL);
return 0;
}
static struct platform_driver spi_imx_driver = {
.driver = {
.name = DRIVER_NAME,
.owner = THIS_MODULE,
},
.id_table = spi_imx_devtype,
.probe = spi_imx_probe,
.remove = __devexit_p(spi_imx_remove),
};
static int __init spi_imx_init(void)
{
return platform_driver_register(&spi_imx_driver);
}
static void __exit spi_imx_exit(void)
{
platform_driver_unregister(&spi_imx_driver);
}
subsys_initcall(spi_imx_init);
module_exit(spi_imx_exit);
MODULE_DESCRIPTION("SPI Master Controller driver");
MODULE_AUTHOR("Sascha Hauer, Pengutronix");
MODULE_LICENSE("GPL");