hi,
Now i has 6-ch cvbs signals which are prcocessed by a ADC(TW6869),then outputs 2 streams of ITU656,one is time multiplexed with 108MHZ(the 4 of 6 cvbs signals),another is time multiplexed with 54MHZ(the 2of 6 cvbs signals).So,can IMX6Q support the 2 streams by its CPI/CSI/MIPI?
If CSI or CPI can,please give me a IC with output port of CSI or CPI.
thanks.
Solved! Go to Solution.
you should parse 6ch stream in sw - fill buffer then separate data, so 180MHz is for
all 6 channels (180/6=30MHz per channel).
I do not read and write in Chinese. :smileyhappy:
Hi 翔 李
yes, it can there are 2xIPU and
sensor (pixel) max. clock frequency 180MHz
IMX6DQCEC Table 67. Sensor Interface Timing Characteristics
Figure 19-1. CSI2IPU gasket connectivity IMX6DQRM
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
HI,
thanks.
In fact,other device will connect the CSI or cpi_mipi of IMX6Q,as well as 6-ch cvbs signal.
I like connect imx6q's nvcc_csi(CSI0_DAT4---CSI0_DAT19 ) with the 6-ch cvbs signal,which is processed by ADC outputs 2 streams of ITU656,one is time multiplexed with 108MHZ(the 4 of 6 cvbs signals),another is time multiplexed with 54MHZ(the 2of 6 cvbs signals).and the nvcc_mipi(csi_0-3_DM/DP) is already used by other device.
IPU CSI input sensor (pixel) max. clock frequency 180MHz
hi,
the max. clock frequency 180MHZ is not meaning "imx6q support the format of time multipexed output(the one itu656 stream includes 6-ch cvbs signal information) .
Some cpu like ti's DM6467 DM3730 can directly connect this multipexed stream,but others like MG3500 can't do unless add a FPGA.
I want to know can the IMX6Q directly connect the multipexed-format stream without adding a FPGA.
Can you read and xrite in Chinese?
我的意思是,
我现在使用IMX6Q设计一款车载产品,我的需求是
1:6路模拟视频输入或者4路百万像素LVDS高清输入。
2:1路800万像素高清LVDS输入。
我现在想使用CSI接口连接800万像素相机,而CPI即MIPI的并口连接6路模拟或者4路LVDS高清(LVDS经过FPGA处理在给IMX6Q)。我想知道,我的6路CVBS模拟信号,经过前端的TW2864等ADC后,输出的一路6合1的复合视频数字流或者1路4合1 1路2合1数字流给IMX6Q的并行MIPI接口,IMX6Q能直接处理这种复合的数字流格式么(一个8bit的ITU656包括有4路或者6路的CVBS信息),我知道TI的DM6467 DM3730等芯片是能直接处理的,但IMX6Q能么?我不想使用模拟的ADC+FPGA方式。
如果CSI接口能的话,请推荐一款前端将模拟视频CVBS转为CSI接口的ADC,能匹配IMX6Q的视频输入接口的。
多谢。
you should parse 6ch stream in sw - fill buffer then separate data, so 180MHz is for
all 6 channels (180/6=30MHz per channel).
I do not read and write in Chinese. :smileyhappy: