can I make a image sd card read only?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

can I make a image sd card read only?

1,621 次查看
gonewithwind-peter
Senior Contributor I

Hi all,

my imx8 boards ,for example , maaxboard and iwave board start up from sd card.

can I make my sd card read only?  if we want to write it, we need to input password.

I know in rootfs /etc /inittab, we can mount it as read only.

but we can use  sd card reader to open the image in it.

 

how I can do?

 

Thank you.

0 项奖励
回复
4 回复数

1,603 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

One way to make it Read-only would be through the physical switch. The other one would require encrypting the data which is what you mentioned. It is necessary to authenticate with the right key to be able to see the data.

 

BR,

Ivan.

0 项奖励
回复

1,594 次查看
gonewithwind-peter
Senior Contributor I

@IvanRuiz 

thank you very much.

 

do you have some more detail or links about your suggestions: "The other one would require encrypting the data which is what you mentioned"

do I need to encrypt the whole image (eg: only rootfs not including kernel ,uboot ),

but after encrypting, how to start up ? (do I need to add some code in kenrel? it seem I need to input password every time to start up)

thank you

0 项奖励
回复

1,572 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

I believe it would be helpful to refer to the following thread where this topic has been addressed: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Encrypted-boot-loader-on-SabreSD-i-MX6q-...

 

Hope it helps!

 

BR

Ivan.

0 项奖励
回复

1,563 次查看
gonewithwind-peter
Senior Contributor I

@IvanRuiz 

thank you

0 项奖励
回复