hi, all
i encountered a problem about camera ov5640.
i checked the boot log. i found the following message.
------------------------------------------------------------------
camera ov5640 is found
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video16
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video17
------------------------------------------------------------------
it seems that the driver is OK.
but when I open the camera APP in android, it display nothing on LVDS panel and it can't preview.
i found the following message in logcat
------------------------------------------------------------------
E/FslCameraHAL( 2208): VIDIOC_STREAMON failed: Operation not permitted
E/FslCameraHAL( 2208): Couldn't start preview for DeviceAdapter
E/FslCameraHAL( 2208): error start stream -1
---------------------------------------------------------------------
and I have checked the following waveform
1)the MCLK pin outputs 24M waveform
2)the HSYNC, VSYNC output square wave
3) CSI0_DAT12~CSI0_DAT19 output waveform
by the way , my resolution of lvds panel is 1024*600, and there is not 1024*600 mode in ov5640_mode_info_data of ov5640 driver
is this a root cause?
Original Attachment has been moved to: camera_android.log.zip
I don't think the resolution is the problem, but we need to rule that out. Do you have a different display with a resolution included in the camera driver?
hi SerchMX
i have not added the other resolution in camera driver.
And i checked the logcat again, i found configuration for ov5640 camera is 640*480 and
it is recommended that media_profiles_480p.xml be used for any board's configuration which defines the that media_profiles_480p.xml be used for any board's configuration which defines the in Android_Frequently_Asked_Questions.pdf .
so as you said, the resolution is not the problem.
Do you solve the problem?