Hi guys,
I have problems about camera performance in imx8qmmek with demo image and with 0v5640 camera sensor and they are all from imx8qmmek evaluation board.
and I have used /unit_test/mx8_v4l2_cap_drm.out with below command:
1. ./mx8_v4l2_cap_drm.out -cam 1 -fmt YUYV -ow 640 -oh 480 -num 300 -p
2. ./mx8_v4l2_cap_drm.out -cam 1 -fmt YUYV -ow 1280 -oh 720 -num 300 -p
3. ./mx8_v4l2_cap_drm.out -cam 1 -fmt YUYV -ow 1920 -oh 1080 -num 300 -p
I expected all each of frame rate is almost 30fps, but acutally.
in case of 640x480, the result is 27fps,
in case of 1080x720 or 1920x1080, the result is 23~25fps.
Why the actual framerate is slower than expected framerate from the nxp document?
Is there any points to enhance the camera framerate?
Please share some of information...
Hello yibhan,
The numbers comes to a camera connected to MIPI, and the latest BSP L5.4..47.
Regards
Hi Bio_TICFSL,
I am using 4.14.98.2.0.0 and I thought ov5640 is reference camera sensor for checking camera performance in bsp.
Hi Bio_TICFSL,
I am using camera module is MINISASTOCSI is nxp's camera module.
Hello,
One can test with nxp version of gstreamer plugins : imx-gst1.0-plugin using
sect.7.3.15 Video conversion on the Linux Guide.
Make sure that you are working with the latest BSP.
it can be posted on gstreamer-imx github page :
https://github.com/Freescale/gstreamer-imx/issues
Regards
Hi BioTICFSL,
1. Do you recommend not to use /mx8_v4l2_cap_drm.out but gstreamer?
If then, give me the reason which you refer to use gstreamer?
2. Tell me the exact version of the lastest BSP? by the way, i am using 4.14.98-2.0.0 BSP version.
Hi BioTCIFSL,
I have something to tell you. A wierd thing is 800x600 frame rate is almost 29 ~ 30 fps.
Do you have any idea about 800x600?