camera frame rate is too low.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

camera frame rate is too low.

1,436 Views
yibhan
Contributor III

Hi guys,

I have concern about cemera performance especially frame rate. I am using UVC(USB Video Class), but I think it doesn't matter.

My board has a frame rate problem, but freescale reference board doesn't.

when camera app is launched, it also take a long time and frame rate is too low. I have used same camera app with my board and freescale board. It is not related with camera app.

I have suspicious logs from dmesg, I have no idea where I should debug some of functions. Please let me guide.

Labels (3)
0 Kudos
Reply
7 Replies

1,343 Views
yibhan
Contributor III

Hi Bio_TICFSL,

I have completed DDR test tools, in my understanding while in tool running, tools are trying to write DDR parameters to DDR.

If so, Could let me know how to rewrite a default DDR parameters to my DDR?

My SOC is imx6qp.

0 Kudos
Reply

1,343 Views
yibhan
Contributor III

Hi Bio_TICFSL,

I am using Kernel_4.14.98, and u-boot source has plugin.s that includes ddr_setting.

Is there any need for me to calculate my ddr parameter?

0 Kudos
Reply

1,343 Views
yibhan
Contributor III

Thank you for answering.

I had already the ddr test results with DDR tools, but I don't know how to adapt them to my device.

Is there any no need to update ddr test results to my device? Or, let guide me in detail.

Thank you for advance.

0 Kudos
Reply

1,343 Views
yibhan
Contributor III

Hello Bio_TICFSL,

I hava ddr test results, but I have no idea where I manually update the test results.

Could you let me know source code location and how to update it?

0 Kudos
Reply

1,343 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Here you see how the ddr stress tool can be used:

https://community.nxp.com/docs/DOC-105652 

0 Kudos
Reply

1,343 Views
yibhan
Contributor III

Hi guy,

I have mistype on previous my comments.

==============================

I have suspicious logs from dmesg,

-> I haven't shown suspicious logs from dmesg.

===============================

0 Kudos
Reply

1,343 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Yibeom,

If your camera is tested with EVB from NXP and it doesn´t seem to be wrong, then you must checked the DDR connections and do:

https://community.nxp.com/docs/DOC-105652 

Regards

0 Kudos
Reply