build/make/core/base_rules.mk:260: error: vendor/nxp/fsl-codec: MODULE.TARGET.SHARED_LIBRARIES.lib_nb_amr_dec_v2_arm9_elinux already defined by android_build/vendor/fsl-codec.
16:46:47 ckati failed with: exit status 1
wei@wei-VirtualBox:~/work/android/imx-p9.0.0_2.3.0$ source imx_android_setup.sh Start fetching the source for android build
Setting REL_PACKAGE_DIR to /home/wei/work/android/imx-p9.0.0_2.3.0
repo: warning: Python 2 is no longer supported; Please upgrade to Python 3.6+.
repo: warning: Python 2 is no longer supported; Please upgrade to Python 3.6+.
Fetching projects: 28% (193/688) platform/packages/providers/UserDictionaryProvFetching projects: 31% (214/688) platform/hardware/qcom/sdm845/thermal
Fetching projects: 100% (688/688), done.
Checking out projects: 42% (289/688) platform/external/python/google-auth-httplChecking out projects: 50% (344/688) platform/external/subsampling-scale-image-Checking out projects: 77% (530/688) platform/packages/apps/SafetyRegulatoryInfChecking out projects: 80% (551/688) platform/packages/providers/ApplicationsPrChecking out projects: 86% (592/688) platform/prebuilts/gcc/linux-x86/arm/arm-lChecking out projects: 100% (688/688), done.
repo sync has finished successfully.
Android source is ready for the build
wei@wei-VirtualBox:~/work/android/imx-p9.0.0_2.3.0/android_build$
Hello Chen,
your question is very similar to the description of the link:
android build fails for MX_O8.0.0_1 sabresd_6dq-userdebug
Check it, please!
In addtion, I have tested P9.0.0_2.3.1 , attachment is detailed steps, for you reference.
Have a nice day!
B.R,
weidong