building u-boot iMX28EVK for NAND flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

building u-boot iMX28EVK for NAND flash

1,386件の閲覧回数
francescoluccon
Contributor I

Hi guys,

I'm involved into a preliminary work for iMX28EVK board and I'm trying to build an u-boot bin file (cross-compiled from an vanilla project)

and installing it through mfg tool.

It seems that using the u-boot.sb (generated at the end of the building) and moving it into the right profile directory, the tool completes the u-boot

installation but resetting the board (just pressing the reset button) the boot-loader doesn't start up.

Have you experienced this problem? How have you solved it?

Thank you in advance, best regards.

Francesco

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,064件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Please check section "3) Installation of U-Boot for a MXS based board to SD card" from:

http://git.denx.de/?p=u-boot.git;a=blob;f=doc/README.mxs;h=5d9e72f958d5ca8c7848d04f5c55e1f2b1f0feac;...

0 件の賞賛
返信

1,064件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Sorry, I meant section "4) Installation of U-Boot into NAND flash on a MX28 based board"

0 件の賞賛
返信