building u-boot iMX28EVK for NAND flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

building u-boot iMX28EVK for NAND flash

1,353 次查看
francescoluccon
Contributor I

Hi guys,

I'm involved into a preliminary work for iMX28EVK board and I'm trying to build an u-boot bin file (cross-compiled from an vanilla project)

and installing it through mfg tool.

It seems that using the u-boot.sb (generated at the end of the building) and moving it into the right profile directory, the tool completes the u-boot

installation but resetting the board (just pressing the reset button) the boot-loader doesn't start up.

Have you experienced this problem? How have you solved it?

Thank you in advance, best regards.

Francesco

标签 (1)
0 项奖励
回复
2 回复数

1,031 次查看
fabio_estevam
NXP Employee
NXP Employee

Please check section "3) Installation of U-Boot for a MXS based board to SD card" from:

http://git.denx.de/?p=u-boot.git;a=blob;f=doc/README.mxs;h=5d9e72f958d5ca8c7848d04f5c55e1f2b1f0feac;...

0 项奖励
回复

1,031 次查看
fabio_estevam
NXP Employee
NXP Employee

Sorry, I meant section "4) Installation of U-Boot into NAND flash on a MX28 based board"

0 项奖励
回复