Dear supporter
We want to redirect the kernel build output to $(TARGET_OUT_INTERMEDIATES)/KERNEL_OBJ
But the below error info occur:
Copy: out/target/product/em70/root/fstab.Partner
Install: out/host/linux-x86/bin/minigzip
Host Clang TableGen: clang (gen-clang-diags-defs -clang-component=Common) <= external/clang/include/clang/Basic/Diagnostic.td
Host Clang TableGen: clang (gen-clang-diags-defs -clang-component=Frontend) <= external/clang/include/clang/Basic/Diagnostic.td
Host Clang TableGen: clang (gen-clang-diags-defs -clang-component=Driver) <= external/clang/include/clang/Basic/Diagnostic.td
firmware/imx/sdma/sdma-imx6q-to1.bin.gen.S: Assembler messages:
firmware/imx/sdma/sdma-imx6q-to1.bin.gen.S:5: Error: file not found: firmware/imx/sdma/sdma-imx6q-to1.bin
CC fs/cramfs/inode.o
CC kernel/power/fbearlysuspend.o
===================== with "make O=" for kernel build =====================================
745 INSTALLED_KERNEL_TARGET := $(PRODUCT_OUT)/kernel
746 TARGET_PREBUILT_KERNEL := $(PRODUCT_OUT)/kernel
747 export KERNEL_OUT := $(TARGET_OUT_INTERMEDIATES)/KERNEL_OBJ
748 KERNEL_CONFIGURE := $(TARGET_OUT_INTERMEDIATES)/KERNEL_OBJ/.config
749 KERNEL_ZIMAGE := $(KERNEL_OUT)/arch/arm/boot/zImage
750 KERNEL_UIMAGE := $(KERNEL_OUT)/arch/arm/boot/uImage
751 KERNEL_HEADERS_INSTALL := $(KERNEL_OUT)/usr
759 $(KERNEL_CONFIGURE): kernel_imx/arch/arm/configs/$(TARGET_KERNEL_DEFCONF)
761 install -d $(KERNEL_OUT)
762 $(MAKE) -C kernel_imx $(TARGET_KERNEL_DEFCONF) -j$(HOST_PROCESSOR) O=../$(KERNEL_O UT) $(KERNEL_ENV)
763
764 $(KERNEL_HEADERS_INSTALL): $(KERNEL_CONFIGURE)
766 install -d $(KERNEL_OUT)
767 $(MAKE) -C kernel_imx -j$(HOST_PROCESSOR) O=../$(KERNEL_OUT) $(KERNEL_ENV) headers _install
768
769 $(TARGET_PREBUILT_KERNEL): $(KERNEL_CONFIGURE)
771 $(MAKE) -C kernel_imx -j$(HOST_PROCESSOR) O=../$(KERNEL_OUT) uImage $(KERNEL_ENV)
772 install -D $(KERNEL_UIMAGE) $(PRODUCT_OUT)/uImage
773 install -D $(KERNEL_ZIMAGE) $(PRODUCT_OUT)/kernel
解決済! 解決策の投稿を見る。
Hi Xingrui zhu,
Me too face similar Issue. Finally, I have built my kernel @ out_dir with small tweak OR change mentioned as bellow...
Check if it works for you..
@ my ./build_kernel.sh
---------------------------------------------------------------------------------------------------
# copy sdma-imx6q-to1.bin to out directory before you compile kernel
cp --parents firmware/imx/sdma/sdma-imx6q-to1.bin $OUT_DIR/
make -j8 ARCH=arm imx6_android_defconfig O=$OUT_DIR
make uImage O=$OUT_DIR
---------------------------------------------------------------------------------------------------
Thanks,
Rajucm
add more info:
Another guy suffer the same issue:
http://boundarydevices.com/new-linux-kernels-for-i-mx6/
quote:
"
It doesn’t seem to be a problem with the source tree, bur rather the makefile rules.
The error only occurs if I build into a separate build tree using ‘make O=’
If I build directly in the Linux source tree, it works fine.
I’ll see if I can figure out why and propose a patch.
"
Hi Xingrui zhu,
Me too face similar Issue. Finally, I have built my kernel @ out_dir with small tweak OR change mentioned as bellow...
Check if it works for you..
@ my ./build_kernel.sh
---------------------------------------------------------------------------------------------------
# copy sdma-imx6q-to1.bin to out directory before you compile kernel
cp --parents firmware/imx/sdma/sdma-imx6q-to1.bin $OUT_DIR/
make -j8 ARCH=arm imx6_android_defconfig O=$OUT_DIR
make uImage O=$OUT_DIR
---------------------------------------------------------------------------------------------------
Thanks,
Rajucm
Thank you.
It does work.