build imx8 kernel fail

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

build imx8 kernel fail

ソリューションへジャンプ
1,714件の閲覧回数
kayiyeh
Contributor II

Dear All,

I am new in this area. I tried to follow the instruction https://www.nxp.com/docs/en/user-guide/i.MX_Yocto_Project_User  to build a imx8qevk image. I followed all the instruction from the beginning step by step and I found imx8mqevk is supported. After executing the fsl-setup-releash.sh described in section 5.1 of the document with MACHINE=imx8mqevk DISTRO=poky, there is no error message. However, I execute  "bitbake core-image-minimal" then an error message shows up immediately said that "imx8mqevk" is not supported. I changed the MACHINE to "imx6slevk" then it works.

Could anyone kindliy tell me what's wrong?

REgards,

Ka-Yi

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
1,411件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Ka-Yi,

Are you using the BSP for L4.9.88_2.0.0? It could be that your repo was initialized to an older BSP which does not support the i.MX8MEVK.

You can download the documentation for this BSP on the link below (you may need to login to download this documentation bundle).

https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.0.0_LINUX_DOCS

I hope this helps!

Regards,

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,412件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Ka-Yi,

Are you using the BSP for L4.9.88_2.0.0? It could be that your repo was initialized to an older BSP which does not support the i.MX8MEVK.

You can download the documentation for this BSP on the link below (you may need to login to download this documentation bundle).

https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.0.0_LINUX_DOCS

I hope this helps!

Regards,

0 件の賞賛
返信